This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

在EVM6678L开发板上加载hua_evmc6678l这个历程,debug调试时,只要不点击 system Reset,运行时控制台就会出现以下错误消息

Other Parts Discussed in Thread: SYSBIOS

控制台输出错误:

QMSS successfully initialized
CPPI successfully initialized
PA successfully initialized
HUA version 2.00.00.04
Setting hostname to tidemo-892345
MAC Address: 90-D7-EB-09-9F-E9
EVM in StaticIP mode at 192.168.2.100
Set IP address of PC to 192.168.2.101
PASS successfully initialized
Ethernet subsystem successfully initialized
Ethernet eventId : 48 and vectId (Interrupt) : 7
Timeout waiting for reply from PA to Pa_addMac command
ti.sysbios.heaps.HeapMem: line 370: assertion failure: A_invalidFree: Invalid free
xdc.runtime.Error.raise: terminating execution

下面是正常运行时的控制台打印的消息

[C66xx_0] QMSS successfully initialized
CPPI successfully initialized
PA successfully initialized
HUA version 2.00.00.04
Setting hostname to tidemo-892345
MAC Address: 90-D7-EB-09-9F-E9
EVM in StaticIP mode at 192.168.2.100
Set IP address of PC to 192.168.2.101
PASS successfully initialized
Ethernet subsystem successfully initialized
Ethernet eventId : 48 and vectId (Interrupt) : 7
Registration of the EMAC Successful, waiting for link up ..
Network Added: If-1:192.168.2.100
Service Status: THTTP : Enabled : : 000

想请教以下红色标记的那条错误是什么意思,我在修改里面NAND FLASH读写的功能时,也会出现这个错误


  • 红色标记提示,可能与释放动态内存时传进去的指针参数为空有关。

    在每次重新加载测试之前,建议点击system reset会对包括core、qmss及外设的复位,否则是有可能运行出错的。

  • 您好

    每次重新加载,点击system reset这样会把DSP主频降为100MHZ吗?

    请您看下这个帖子 http://www.deyisupport.com/question_answer/dsp_arm/c6000_multicore/f/53/t/29895.aspx  提及到会降低主频。

    如果直接断电重启,应该就不会存在需要system reset了吧。