控制台输出错误:
QMSS successfully initialized
CPPI successfully initialized
PA successfully initialized
HUA version 2.00.00.04
Setting hostname to tidemo-892345
MAC Address: 90-D7-EB-09-9F-E9
EVM in StaticIP mode at 192.168.2.100
Set IP address of PC to 192.168.2.101
PASS successfully initialized
Ethernet subsystem successfully initialized
Ethernet eventId : 48 and vectId (Interrupt) : 7
Timeout waiting for reply from PA to Pa_addMac command
ti.sysbios.heaps.HeapMem: line 370: assertion failure: A_invalidFree: Invalid free
xdc.runtime.Error.raise: terminating execution
下面是正常运行时的控制台打印的消息
[C66xx_0] QMSS successfully initialized
CPPI successfully initialized
PA successfully initialized
HUA version 2.00.00.04
Setting hostname to tidemo-892345
MAC Address: 90-D7-EB-09-9F-E9
EVM in StaticIP mode at 192.168.2.100
Set IP address of PC to 192.168.2.101
PASS successfully initialized
Ethernet subsystem successfully initialized
Ethernet eventId : 48 and vectId (Interrupt) : 7
Registration of the EMAC Successful, waiting for link up ..
Network Added: If-1:192.168.2.100
Service Status: THTTP : Enabled : : 000
想请教以下红色标记的那条错误是什么意思,我在修改里面NAND FLASH读写的功能时,也会出现这个错误