本文以VPSS M3为例,介绍了如何使用CCS v5调试DM81XX的M3代码,同时该调试思想也适用于其他的M3模块,以及DSP的调试
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
本文以VPSS M3为例,介绍了如何使用CCS v5调试DM81XX的M3代码,同时该调试思想也适用于其他的M3模块,以及DSP的调试
Zhenyu Zhu 说:我这边关联不到源码怎么办
请确认你编译使用的是debug模式,并且没有用strip把symbol的信息去除掉。一般debug模式下编译出来的文件都有十几MB。
你好,
图片太模糊。请确认你使用的xem3文件和你的c代码是匹配的。你是把你使用的代码从Linux复制到window?
stripe在编译器的bin目录下,下面是help信息。实际使用的代码会用stripe把symbol等debug信息去掉,这样可执行文件可以减少到2M左右。
C:\CCSv5\ccsv5\tools\compiler\TMS470_4.5.1\bin>strip470.exe -h
TMS470 Strip Utility v4.5.1
Tools Copyright (c) 1996-2008 Texas Instruments Incorporated
Usage: strip470.exe [-options] filename
Use 'strip470.exe -h <option>' for more information on a particular option. Use
'strip470.exe -h <text>' to search options for information regarding <text>.
Option arguments surrounded by [] declare they are optional. Option arguments
separated by commas specify that the option's argument must be chosen from
those arguments listed.
General Options:
-h Display help
-o=file Write stripped output to a new file
-p Strip additional info from a linked object file.
Alice Liu1
我在您提供的指导文件的指引下,能够成功的在ccs下仿真M3的程序。在此,首先表示感谢!!
我目前碰到的问题是,在仿真过程中,查看全局性质的结构体以及成员变量的值,提示“Error:identifier not found:Ipc_module”.
此次用的的模式dvr-rdk/mcf/src-bios6/main_app/MAIN_APP_m3vpss.c。查看的变量Ipc_module定义在ti_tools/syslink/syslink_2_20_02_20/packages/ti/syslink/ipc/hlos/knl/ipc.c。
静候您、以及其他有经验的人回复!