Other Parts Discussed in Thread: AM625, TSC2007
SDK版本08.03.00.19,已经安装如下图的说明禁用gpu了,但是目前文件系统无法启动,请问文件系统怎么修改可以适配6231

报错如下,一直卡在如下位置
[ 14.803125] max_p2p_conn = 8, max_sta_conn = 8 Starting Load/Save RF Kill Switch Status...
[ 14.849629] wlan: version = SD8987---16.92.10.p208-MXM5X16210-GPL-(FP92)
[ 14.859212] wlan: Driver loaded successfully
[ OK ] Started Load/Save RF Kill Switch Status.
[ *** ] A start job is running for udev Wai…ice Initialization (30s / 3min 2s)