This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5K2E04 的两组PCIE 接口,每组有2个lan。是否能够支持每一个lan挂一个从器件?

Other Parts Discussed in Thread: AM5K2E04

您好,

AM5K2E04 有两组PCIE接口,每组有2个lan。是否能够支持每一个lan挂一个从器件

  • 不可以,每个PCIE只有一个port,每个port可以工作在 x1或x2 mode,PCIe外面可以接switch,通过switch达到与多个设备连接。

  • 您好,我用的是c66ak2e05的评估板evmk2e,现在安装上了ccs和MCDSK,看了很多TI公司的说明文件,但是还是不知道从哪开始,怎么着手开始开发程序,您能帮帮我吗?

    目前存在的问题:

    1、建立工程时,相应的库文件、头文件的位置在哪。我在安装路径下的文件夹里找到了不只一个路径,不知道那个是对的

    2、建立工程时,找不到对应的cmd文件

    3、建立工程时,RSTC选项卡中,有target和platform选项,是空白的,没有下拉菜单。是我软件安装错了吗?不知道怎么填?

    4、建立的工程不输出.out文件。

    5、生成.out文件的debug也不成功

    现在遇到了很多问题,您能提供一些基础的教程吗?指导一步步进行操作的那种。如果方便的话,可以加您好友或邮箱吗