您好,
AM5K2E04 有两组PCIE接口,每组有2个lan。是否能够支持每一个lan挂一个从器件
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,我用的是c66ak2e05的评估板evmk2e,现在安装上了ccs和MCDSK,看了很多TI公司的说明文件,但是还是不知道从哪开始,怎么着手开始开发程序,您能帮帮我吗?
目前存在的问题:
1、建立工程时,相应的库文件、头文件的位置在哪。我在安装路径下的文件夹里找到了不只一个路径,不知道那个是对的
2、建立工程时,找不到对应的cmd文件
3、建立工程时,RSTC选项卡中,有target和platform选项,是空白的,没有下拉菜单。是我软件安装错了吗?不知道怎么填?
4、建立的工程不输出.out文件。
5、生成.out文件的debug也不成功
现在遇到了很多问题,您能提供一些基础的教程吗?指导一步步进行操作的那种。如果方便的话,可以加您好友或邮箱吗