This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你的显示指的是VPBE口输出BT1120这种显示吗?
你看过你显示输出的实际分辨率是不是200w?
还有就是你目前看到的图像,是一个完整的想要显示的图像还是说只图像往右下方移动了的结果?
我们是做的网络摄像机,用100万像素,720P的就可以显示OK。。。用200万像素,1080P_D1,显示效果就有部分显示黑色的。。。。网络传输数据到PC服务端端软件,怀疑是分辨率的问题,我将av_capture/application/ipnc/av_server/src/common/avServerUi.c里的config->captureConfig[i].width = (gAVSERVER_UI_config.mode==AVSERVER_UI_CAPTURE_MODE_1080P_D1)?720:320;修改改成640:320;
onfig->encodeConfig[i].cropWidth = (gAVSERVER_UI_config.mode==AVSERVER_UI_CAPTURE_MODE_1080P_D1)?720:320;修改改成640:320;运行程序出错
我们是做的网络摄像机,用100万像素,720P的就可以显示OK。。。用200万像素,1080P_D1,显示效果就有部分显示黑色的。。。。网络传输数据到PC服务端端软件,怀疑是分辨率的问题,我将av_capture/application/ipnc/av_server/src/common/avServerUi.c里的config->captureConfig[i].width = (gAVSERVER_UI_config.mode==AVSERVER_UI_CAPTURE_MODE_1080P_D1)?720:320;修改改成640:320; onfig->encodeConfig[i].cropWidth = (gAVSERVER_UI_config.mode==AVSERVER_UI_CAPTURE_MODE_1080P_D1)?720:320;修改改成640:320;运行程序出错