This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BB-black 网口问题

Other Parts Discussed in Thread: AM3359

各位大神:

         本人按照BB-black自己做了一块板子,除了将原来使用的网口1修改为使用网口2以外,别的完全一样,现在网口2采用的是RMII模式,网口PHY芯片LAN8710A的输入时钟和AM3359的REF_CLK同时连接到50MHz的有源晶振上,而且测试PHY芯片工作正常,自动协商工作也能正常完成,现在遇到的问题是PCping不通板子。我的程序之前是在BB-black开发板上调试通的(采用MII模式),然后移植过来就修改了一下pinmux和网口模式(将MII修改为RMII ),不知道网口1和网口2还有其他不同的地方吗,或者RMII模式配置需要注意些什么?请大神给点排查建议或者指点一下,我将不胜感激,附上CPSW部分的配置程序。如下:

 

  • 我是在sys/bios下跑的NDK,顺便问一下,如果是port2的话,这块如何配置?

  • 补充一下:我这边做了一些测试,发现:NDK功能正常,可以读出MAC地址和分配的静态IP;PHY的寄存器中的值也正常,自动协商也完成了,现在我怀疑是NDK的配置出问题了,就是在NDK配置时没有注意选的是网口1还是网口2,所以才会使我所使用的AM3359的网口2与PHY芯片没有对应起来才导致这种情况的,所以我就想问问,NDK的配置(图形化配置)中,有涉及到选择网口1或者网口2的地方吗?