This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x 网口芯片从 AR8035 改为 LAN8710, 无法ping通

大家好,

         参照EBEST的DEVKIT8600和BeagleBone的设计, 将DEVKIT8600上的PHY由AR8035更改为LAN8710,不知软件哪些地方要做修改。

谢谢!

  • 我们TI发布的SDK软件包里面包含了对beaglebone支持,包含了LAN8710的driver。

  • 用的什么接口 rmii还是mii  gmii_sel改没改 mac_control改没改 pinmux做没做 phy_id改没改

  • beaglebone上的8710是MII模式的,你的硬件是参考beaglebone做的吗?

  • 由于TI的SDK包中使用的general PHY driver,所以修改很简单,更明确地说,是确认配置。

    使用LAN8710,可以在u-boot中配置板子类型的使用调用beaglebone的配置,前提是MII接口。如果换成RMII,则需要修改PINMUX.

    妥当一些的话,就照着如下部分进行检查:

    如u-boot下主要确认三点:

    1)Program GMII_SEL in control module with 0x5 for RMII Interface

    2)Pinmux configuration to support rmii interface

    3)Phy ID setting in Platform data(由PHY的硬件电路决定,通过在PHY_ID的三个管脚上下拉来决定)

    Linux下调试也是确认以上三点

  • 我也是使用LAN8710 RMII。可是uboot就是打印phy not found ,我调试打印信息,mdio扫描,phy没有应答。可以提供一份lan8710 RMII的应用实例吗?

  • 我采用RMII连接方式,把lan8710a的3个phy id引脚全下拉,那软件上在哪里改id,内核为3.14.43?现在内核打印id号为net eth0: phy found : id is : 0x7c0f1

    这正常吗?正在能ping能,但是测试丢包率很大。在u-boot下tftp也会卡住,无法传文件。

     iperf -s -u -i 2
    ------------------------------------------------------------
    Server listening on UDP port 5001
    Receiving 1470 byte datagrams
    UDP buffer size:  208 KByte (default)
    ------------------------------------------------------------
    [  3] local 192.168.1.72 port 5001 connected with 192.168.1.235 port 43667
    [ ID] Interval       Transfer     Bandwidth        Jitter   Lost/Total Datagrams
    [  3]  0.0- 2.0 sec  22.5 MBytes  94.5 Mbits/sec   0.255 ms  197/16276 (1.2%)
    [  3]  2.0- 4.0 sec  22.0 MBytes  92.1 Mbits/sec   0.166 ms  616/16277 (3.8%)
    [  3]  4.0- 6.0 sec  22.8 MBytes  95.7 Mbits/sec   0.077 ms    2/16276 (0.012%)
    [  3]  6.0- 8.0 sec  22.8 MBytes  95.7 Mbits/sec   0.113 ms    1/16275 (0.0061%)
    [  3]  8.0-10.0 sec  22.8 MBytes  95.7 Mbits/sec   0.093 ms    4/16278 (0.025%)
    [  3] 10.0-12.0 sec  22.8 MBytes  95.7 Mbits/sec   0.209 ms    2/16276 (0.012%)
    [  3] 12.0-14.0 sec  22.8 MBytes  95.6 Mbits/sec   0.088 ms    6/16272 (0.037%)
    [  3] 14.0-16.0 sec  22.2 MBytes  92.9 Mbits/sec   0.090 ms  479/16279 (2.9%)
    [  3] 16.0-18.0 sec  22.8 MBytes  95.7 Mbits/sec   0.140 ms    6/16274 (0.037%)
    [  3] 18.0-20.0 sec  22.8 MBytes  95.6 Mbits/sec   0.347 ms   16/16277 (0.098%)
    [  3] 20.0-22.0 sec  21.9 MBytes  92.0 Mbits/sec   0.087 ms  627/16281 (3.9%)
    [  3] 22.0-24.0 sec  22.5 MBytes  94.4 Mbits/sec   0.156 ms  227/16276 (1.4%)
    [  3] 24.0-26.0 sec  22.8 MBytes  95.6 Mbits/sec   0.069 ms   14/16276 (0.086%)
    [  3] 26.0-28.0 sec  22.8 MBytes  95.5 Mbits/sec   0.189 ms   29/16277 (0.18%)
    [  3] 28.0-30.0 sec  21.6 MBytes  90.5 Mbits/sec   0.078 ms  891/16276 (5.5%)
    [  3] 30.0-32.0 sec  21.3 MBytes  89.4 Mbits/sec   0.101 ms 1064/16276 (6.5%)
    [  3] 32.0-34.0 sec  21.9 MBytes  91.7 Mbits/sec   0.251 ms  681/16277 (4.2%)
    [  3] 34.0-36.0 sec  22.5 MBytes  94.5 Mbits/sec   0.191 ms  204/16277 (1.3%)
    [  3] 36.0-38.0 sec  21.7 MBytes  91.1 Mbits/sec   0.085 ms  786/16276 (4.8%)
    [  3] 38.0-40.0 sec  22.2 MBytes  93.0 Mbits/sec   0.136 ms  460/16276 (2.8%)
    [  3] 40.0-42.0 sec  22.1 MBytes  92.9 Mbits/sec   0.168 ms  480/16277 (2.9%)
    [  3] 42.0-44.0 sec  22.8 MBytes  95.6 Mbits/sec   0.075 ms    9/16276 (0.055%)
    [  3] 44.0-46.0 sec  22.2 MBytes  92.9 Mbits/sec   0.106 ms  473/16277 (2.9%)
    [  3] 46.0-48.0 sec  22.8 MBytes  95.6 Mbits/sec   0.263 ms    9/16276 (0.055%)
    [  3] 48.0-50.0 sec  22.8 MBytes  95.7 Mbits/sec   0.129 ms    4/16277 (0.025%)
    [  3] 50.0-52.0 sec  22.5 MBytes  94.3 Mbits/sec   0.072 ms  247/16276 (1.5%)
    [  3] 52.0-54.0 sec  22.8 MBytes  95.7 Mbits/sec   0.187 ms    4/16277 (0.025%)
    [  3] 54.0-56.0 sec  22.8 MBytes  95.6 Mbits/sec   0.226 ms    6/16262 (0.037%)
    [  3] 56.0-58.0 sec  22.6 MBytes  94.7 Mbits/sec   0.143 ms  184/16290 (1.1%)
    [  3] 58.0-60.0 sec  22.8 MBytes  95.7 Mbits/sec   0.126 ms    2/16276 (0.012%)
    [  3]  0.0-60.0 sec   674 MBytes  94.2 Mbits/sec   0.380 ms 7729/488357 (1.6%)

    [  3]  0.0-60.0 sec  1 datagrams received out-of-order

  • 我们驱动中,SKEVM板上默认的PHY_ID就是设置为0的,在RGMII1上。RGMII2的PHY_ID是2,如果没有第二个网口就没所谓了。

    你的情况不像是PHY_ID设置错误,如果是PHY_ID设置错误的话,你应该是通讯不上的。现在丢包率比较高,但是能ping通的话。

    我建议先确认硬件山上的几个设计:一个是时钟是否使用的外部,一个是布线是否遵循的上面提到的一些规则。软件上能做的测试话,可以尝试把自协商固定为10M来通讯,如果这样丢包率明显小了,或者能TFTP了,能从一定程度上说明这个板子目前的通路和驱动是好的,但是可能由于信号完整性等问题导致通讯失败,需从硬件上进行改善。

  • 嗯,原来phy_ID是多网卡用的啊。我们也猜测是硬件问题,有关于phy布线要求的相关资料吗?谢谢。另外如何强制10M通讯,我在u-boot中添加代码:

        const char *devname;
        u32 reg;
        devname = miiphy_get_current_dev();
        miiphy_read(devname,0,LAN8710_PHY_Special_Modes_ADDR_REG,&reg);
        reg &= ~(0x7 << 5);
        reg |= (0x1 << 5);// 10M
        miiphy_write(devname,0,LAN8710_PHY_Special_Modes_ADDR_REG,reg);
        printf("lan8710 mode =  0x%x \n", reg);

    但是,ping的时候仍然显示 使用100M传输。

    link up on port 0, speed 100, full duplex
    Using cpsw device
    host 192.168.1.72 is alive

  • 关于PHY这块的布线设计的话,一般是根据PHY芯片厂商提供的手册来进行。

    像TI的DP83848,可以参考这个链接里面的介绍:http://www.deyisupport.com/question_answer/dsp_arm/sitara_arm/f/25/t/45981.aspx

    还有一个参考就是DATASHEET手册。

    强制改10M的话,印象中是用MDIO write的方式来写PHY侧的寄存器,来指定他工作的方式。

    以DP83848为例,在BMCR的12 bit就可以把这个关掉,在13 bit进行设置。