大家好,
参照EBEST的DEVKIT8600和BeagleBone的设计, 将DEVKIT8600上的PHY由AR8035更改为LAN8710,不知软件哪些地方要做修改。
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
大家好,
参照EBEST的DEVKIT8600和BeagleBone的设计, 将DEVKIT8600上的PHY由AR8035更改为LAN8710,不知软件哪些地方要做修改。
谢谢!
由于TI的SDK包中使用的general PHY driver,所以修改很简单,更明确地说,是确认配置。
使用LAN8710,可以在u-boot中配置板子类型的使用调用beaglebone的配置,前提是MII接口。如果换成RMII,则需要修改PINMUX.
妥当一些的话,就照着如下部分进行检查:
如u-boot下主要确认三点:
1)Program GMII_SEL in control module with 0x5 for RMII Interface
2)Pinmux configuration to support rmii interface
3)Phy ID setting in Platform data(由PHY的硬件电路决定,通过在PHY_ID的三个管脚上下拉来决定)
Linux下调试也是确认以上三点
我采用RMII连接方式,把lan8710a的3个phy id引脚全下拉,那软件上在哪里改id,内核为3.14.43?现在内核打印id号为net eth0: phy found : id is : 0x7c0f1
这正常吗?正在能ping能,但是测试丢包率很大。在u-boot下tftp也会卡住,无法传文件。
iperf -s -u -i 2
------------------------------------------------------------
Server listening on UDP port 5001
Receiving 1470 byte datagrams
UDP buffer size: 208 KByte (default)
------------------------------------------------------------
[ 3] local 192.168.1.72 port 5001 connected with 192.168.1.235 port 43667
[ ID] Interval Transfer Bandwidth Jitter Lost/Total Datagrams
[ 3] 0.0- 2.0 sec 22.5 MBytes 94.5 Mbits/sec 0.255 ms 197/16276 (1.2%)
[ 3] 2.0- 4.0 sec 22.0 MBytes 92.1 Mbits/sec 0.166 ms 616/16277 (3.8%)
[ 3] 4.0- 6.0 sec 22.8 MBytes 95.7 Mbits/sec 0.077 ms 2/16276 (0.012%)
[ 3] 6.0- 8.0 sec 22.8 MBytes 95.7 Mbits/sec 0.113 ms 1/16275 (0.0061%)
[ 3] 8.0-10.0 sec 22.8 MBytes 95.7 Mbits/sec 0.093 ms 4/16278 (0.025%)
[ 3] 10.0-12.0 sec 22.8 MBytes 95.7 Mbits/sec 0.209 ms 2/16276 (0.012%)
[ 3] 12.0-14.0 sec 22.8 MBytes 95.6 Mbits/sec 0.088 ms 6/16272 (0.037%)
[ 3] 14.0-16.0 sec 22.2 MBytes 92.9 Mbits/sec 0.090 ms 479/16279 (2.9%)
[ 3] 16.0-18.0 sec 22.8 MBytes 95.7 Mbits/sec 0.140 ms 6/16274 (0.037%)
[ 3] 18.0-20.0 sec 22.8 MBytes 95.6 Mbits/sec 0.347 ms 16/16277 (0.098%)
[ 3] 20.0-22.0 sec 21.9 MBytes 92.0 Mbits/sec 0.087 ms 627/16281 (3.9%)
[ 3] 22.0-24.0 sec 22.5 MBytes 94.4 Mbits/sec 0.156 ms 227/16276 (1.4%)
[ 3] 24.0-26.0 sec 22.8 MBytes 95.6 Mbits/sec 0.069 ms 14/16276 (0.086%)
[ 3] 26.0-28.0 sec 22.8 MBytes 95.5 Mbits/sec 0.189 ms 29/16277 (0.18%)
[ 3] 28.0-30.0 sec 21.6 MBytes 90.5 Mbits/sec 0.078 ms 891/16276 (5.5%)
[ 3] 30.0-32.0 sec 21.3 MBytes 89.4 Mbits/sec 0.101 ms 1064/16276 (6.5%)
[ 3] 32.0-34.0 sec 21.9 MBytes 91.7 Mbits/sec 0.251 ms 681/16277 (4.2%)
[ 3] 34.0-36.0 sec 22.5 MBytes 94.5 Mbits/sec 0.191 ms 204/16277 (1.3%)
[ 3] 36.0-38.0 sec 21.7 MBytes 91.1 Mbits/sec 0.085 ms 786/16276 (4.8%)
[ 3] 38.0-40.0 sec 22.2 MBytes 93.0 Mbits/sec 0.136 ms 460/16276 (2.8%)
[ 3] 40.0-42.0 sec 22.1 MBytes 92.9 Mbits/sec 0.168 ms 480/16277 (2.9%)
[ 3] 42.0-44.0 sec 22.8 MBytes 95.6 Mbits/sec 0.075 ms 9/16276 (0.055%)
[ 3] 44.0-46.0 sec 22.2 MBytes 92.9 Mbits/sec 0.106 ms 473/16277 (2.9%)
[ 3] 46.0-48.0 sec 22.8 MBytes 95.6 Mbits/sec 0.263 ms 9/16276 (0.055%)
[ 3] 48.0-50.0 sec 22.8 MBytes 95.7 Mbits/sec 0.129 ms 4/16277 (0.025%)
[ 3] 50.0-52.0 sec 22.5 MBytes 94.3 Mbits/sec 0.072 ms 247/16276 (1.5%)
[ 3] 52.0-54.0 sec 22.8 MBytes 95.7 Mbits/sec 0.187 ms 4/16277 (0.025%)
[ 3] 54.0-56.0 sec 22.8 MBytes 95.6 Mbits/sec 0.226 ms 6/16262 (0.037%)
[ 3] 56.0-58.0 sec 22.6 MBytes 94.7 Mbits/sec 0.143 ms 184/16290 (1.1%)
[ 3] 58.0-60.0 sec 22.8 MBytes 95.7 Mbits/sec 0.126 ms 2/16276 (0.012%)
[ 3] 0.0-60.0 sec 674 MBytes 94.2 Mbits/sec 0.380 ms 7729/488357 (1.6%)
[ 3] 0.0-60.0 sec 1 datagrams received out-of-order
我们驱动中,SKEVM板上默认的PHY_ID就是设置为0的,在RGMII1上。RGMII2的PHY_ID是2,如果没有第二个网口就没所谓了。
你的情况不像是PHY_ID设置错误,如果是PHY_ID设置错误的话,你应该是通讯不上的。现在丢包率比较高,但是能ping通的话。
我建议先确认硬件山上的几个设计:一个是时钟是否使用的外部,一个是布线是否遵循的上面提到的一些规则。软件上能做的测试话,可以尝试把自协商固定为10M来通讯,如果这样丢包率明显小了,或者能TFTP了,能从一定程度上说明这个板子目前的通路和驱动是好的,但是可能由于信号完整性等问题导致通讯失败,需从硬件上进行改善。
嗯,原来phy_ID是多网卡用的啊。我们也猜测是硬件问题,有关于phy布线要求的相关资料吗?谢谢。另外如何强制10M通讯,我在u-boot中添加代码:
const char *devname;
u32 reg;
devname = miiphy_get_current_dev();
miiphy_read(devname,0,LAN8710_PHY_Special_Modes_ADDR_REG,®);
reg &= ~(0x7 << 5);
reg |= (0x1 << 5);// 10M
miiphy_write(devname,0,LAN8710_PHY_Special_Modes_ADDR_REG,reg);
printf("lan8710 mode = 0x%x \n", reg);
但是,ping的时候仍然显示 使用100M传输。
link up on port 0, speed 100, full duplex
Using cpsw device
host 192.168.1.72 is alive
关于PHY这块的布线设计的话,一般是根据PHY芯片厂商提供的手册来进行。
像TI的DP83848,可以参考这个链接里面的介绍:http://www.deyisupport.com/question_answer/dsp_arm/sitara_arm/f/25/t/45981.aspx
还有一个参考就是DATASHEET手册。
强制改10M的话,印象中是用MDIO write的方式来写PHY侧的寄存器,来指定他工作的方式。
以DP83848为例,在BMCR的12 bit就可以把这个关掉,在13 bit进行设置。