本人在将6416 DSP 的EMIF 接口配置为 8位同步 的情况下,
分别将EDMA 的ESIZE 配置为 8位和32位,
利用EDMA从挂接在EMIF接口的外部32位同步存储器中去读320*256个数据到DSP内存时,
发现EDMA 发出的CE片选信号区别很大:
ESIZE 为8位时,CE片选信号间隔有效;
ESIZE为32位时,CE片选信号持续有效。
想请教各位论坛里面的高手,导致这一现象的原因。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.