This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6416 DSP 在EMIF为8位的情况下,将EDMA ESIZE 配置为8 位和32 位时,两者之间硬件上读时序的区别



本人在将6416 DSP 的EMIF 接口配置为 8位同步 的情况下,

分别将EDMA 的ESIZE 配置为 8位和32位,

利用EDMA从挂接在EMIF接口的外部32位同步存储器中去读320*256个数据到DSP内存时,

发现EDMA 发出的CE片选信号区别很大:

ESIZE 为8位时,CE片选信号间隔有效;

ESIZE为32位时,CE片选信号持续有效。

想请教各位论坛里面的高手,导致这一现象的原因。