請問..
我們的板子AM3352, 使用linux SDK6.0 在uboot 初始化PHY時
總會出現 PHY reset timed out 訊息,且在uboot,或進入rootfs後 網路無法使用
但若我休息一陣子在開機,進入uboot或進入rootfs後 網路都可以正確使用100M/1000M 都正確 (長時間使用也都正確)
但只要重開機,又是一樣現象 PHY reset timed out
休息一陣子在開又正常
請問這會是什麼問題造成???
p/s:我已經有修改phy.c timeout時間為5秒,仍然是會timeout
U-Boot 2013.01.01 (Apr 21 2014 - 14:04:26)
I2C: ready
DRAM: 256 MiB
WARNING: Caches not enabled
NAND: No NAND device found!!!
0 MiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
*** Warning - readenv() failed, using default environment
musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO
Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
USB Peripheral mode controller at 47401000 using PIO, IRQ 0
musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO
Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
USB Host mode controller at 47401800 using PIO, IRQ 0
Net: <ethaddr> not set. Validating first E-fuse MAC
PHY reset timed out
cpsw, usb_ether
Hit any key to stop autoboot: 0
mmc0 is current device
SD/MMC found on device 0