This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PHY reset timed out

Expert 2272 points

Other Parts Discussed in Thread: AM3352

請問..

我們的板子AM3352, 使用linux SDK6.0 在uboot 初始化PHY時

總會出現  PHY reset timed out 訊息,且在uboot,或進入rootfs後 網路無法使用

但若我休息一陣子在開機,進入uboot或進入rootfs後 網路都可以正確使用100M/1000M 都正確 (長時間使用也都正確)

但只要重開機,又是一樣現象 PHY reset timed out

休息一陣子在開又正常

請問這會是什麼問題造成???

p/s:我已經有修改phy.c  timeout時間為5秒,仍然是會timeout

U-Boot 2013.01.01 (Apr 21 2014 - 14:04:26)

I2C: ready
DRAM: 256 MiB
WARNING: Caches not enabled
NAND: No NAND device found!!!
0 MiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
*** Warning - readenv() failed, using default environment

musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO
Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
USB Peripheral mode controller at 47401000 using PIO, IRQ 0
musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO
Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
USB Host mode controller at 47401800 using PIO, IRQ 0
Net: <ethaddr> not set. Validating first E-fuse MAC
PHY reset timed out
cpsw, usb_ether
Hit any key to stop autoboot: 0
mmc0 is current device
SD/MMC found on device 0