我在画368的原理图时,有些引脚不知道该如何处理,在看了datasheet和对应的application note后仍然存在疑问。所以在这里咨询一下大家,具体如下:
1. ADC
我不清楚ADC_CH0~ADC_CH5这六个引脚该如何连接。因为我不确定这六个引脚的功能。我个人的理解是这六个引脚368ADC的6个输入通道。具体选择哪个通道进行AD转换可以控制寄存器修改。那么硬件角度看,这几个引脚需要连接到哪里呢?我觉得需要用到ADC的地方会有音频输入(MIC),但是368有特定的引脚连接MIC,似乎和ADC没有多少联系啊!所以不知道ADC_CH0~ADC_CH5该如何正确连接了。
2. RTC
368的RTC有11个可配置的GIO,这些引脚可以用来做什么呢?如果不用这些引脚的话,该如何处理呢?连接到GND或者电源或是FLOATING?
3. JTAG
368的JTAG接口有什么作用呢?从负责368软体的同事说,可以通过JTAG接口将系统镜像文件烧写到FLASH中去。那如果我们不需要这个功能的话,是否可以将JTAG的全部接口都做FLOATING处理呢?因为所画的电路板面积很有限。
4. Oscillator ground PIN(VSS_MX1和VSS_32K)和VSSA
根据368datasheet上的描述,引脚VSS_MX1和VSS_32K只连接到晶体负载电容的ground而不要连接到其他的电路或模块的ground,是这样的吗?
根据368的datasheet的Page72最下面的注释3说到:“For proper device operation, keep this pin separate from digital ground.”其意思是VSSA引脚需要与VSS引脚进行隔离吗?用一颗磁珠隔离是否可以?