This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM368的若干引脚连接问题,请大家帮忙!



我在画368的原理图时,有些引脚不知道该如何处理,在看了datasheet和对应的application note后仍然存在疑问。所以在这里咨询一下大家,具体如下:

1. ADC

我不清楚ADC_CH0~ADC_CH5这六个引脚该如何连接。因为我不确定这六个引脚的功能。我个人的理解是这六个引脚368ADC的6个输入通道。具体选择哪个通道进行AD转换可以控制寄存器修改。那么硬件角度看,这几个引脚需要连接到哪里呢?我觉得需要用到ADC的地方会有音频输入(MIC),但是368有特定的引脚连接MIC,似乎和ADC没有多少联系啊!所以不知道ADC_CH0~ADC_CH5该如何正确连接了。

2. RTC

368的RTC有11个可配置的GIO,这些引脚可以用来做什么呢?如果不用这些引脚的话,该如何处理呢?连接到GND或者电源或是FLOATING?

3. JTAG

368的JTAG接口有什么作用呢?从负责368软体的同事说,可以通过JTAG接口将系统镜像文件烧写到FLASH中去。那如果我们不需要这个功能的话,是否可以将JTAG的全部接口都做FLOATING处理呢?因为所画的电路板面积很有限。

4. Oscillator ground PIN(VSS_MX1和VSS_32K)和VSSA

根据368datasheet上的描述,引脚VSS_MX1和VSS_32K只连接到晶体负载电容的ground而不要连接到其他的电路或模块的ground,是这样的吗?

根据368的datasheet的Page72最下面的注释3说到:“For proper device operation, keep this pin separate from digital ground.”其意思是VSSA引脚需要与VSS引脚进行隔离吗?用一颗磁珠隔离是否可以?

  • 1. ADC

    我不清楚ADC_CH0~ADC_CH5这六个引脚该如何连接。因为我不确定这六个引脚的功能。我个人的理解是这六个引脚368ADC的6个输入通道。具体选择哪个通道进行AD转换可以控制寄存器修改。那么硬件角度看,这几个引脚需要连接到哪里呢?我觉得需要用到ADC的地方会有音频输入(MIC),但是368有特定的引脚连接MIC,似乎和ADC没有多少联系啊!所以不知道ADC_CH0~ADC_CH5该如何正确连接了。

    [Eason]  ADC 的作用很广泛,看你怎么运用了 。比如拿来测温,测光等等。   不用的时候的接法,手册上写的很清楚


    2. RTC

    368的RTC有11个可配置的GIO,这些引脚可以用来做什么呢?如果不用这些引脚的话,该如何处理呢?连接到GND或者电源或是FLOATING?

    [Eason]  不用的话输出口悬空,输入口接电阻到地。


    3. JTAG

    368的JTAG接口有什么作用呢?从负责368软体的同事说,可以通过JTAG接口将系统镜像文件烧写到FLASH中去。那如果我们不需要这个功能的话,是否可以将JTAG的全部接口都做FLOATING处理呢?因为所画的电路板面积很有限。

    [Eason]  JTAG 口是要用来做调试用的。在设计初期一定要留。  


    4. Oscillator ground PIN(VSS_MX1和VSS_32K)和VSSA

    根据368datasheet上的描述,引脚VSS_MX1和VSS_32K只连接到晶体负载电容的ground而不要连接到其他的电路或模块的ground,是这样的吗?

    根据368的datasheet的Page72最下面的注释3说到:“For proper device operation, keep this pin separate from digital ground.”其意思是VSSA引脚需要与VSS引脚进行隔离吗?用一颗磁珠隔离是否可以?

    [Eason] 是的。隔离一下为好。