TVP5158,设置I2C后,只输出无视频状态下的黑色背景色,接入视频信号也一直无图像输出,查看状态寄存器也没有相关的视频信息。而且可以看到输出的图像帧率变低。请问这是怎么回事?
我是使用PORTA单路D1输出,下面是寄存器的设置,未设置到的,都是使用芯片默认值。
0XB0, 0X00, /*AVD输出控制1*/
0XB1, 0X10, /*AVD输出控制2*/
0XB2, 0X27, /*AVD输出控制2*/
0XB3, 0XE4, /*OFM通道选择1*/
0XB4, 0XE4, /*OFM通道选择2*/
0XB5, 0X00, /*OFM通道选择3*/
0XB6, 0X1B,
0XB7, 0X04,
0XB8, 0X40,
0XB9, 0X00,
0XBA, 0X01,
请问是寄存器配置的问题吗?我的邮箱long_eiffel@126.com,期待你的帮助。谢谢!