This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8168从SD卡烧写到nand



我用的是闻亭做的DM8168的板子。情况是这样的:

1.SD已经能正常启动,我想从SD烧写到nand,在uboot状态下我输入mmc init,没反应,接下来fatload mmc 1 0x81000000 uImage也是没法执行的。

2.我从nandflash启动到uboot状态,然后出入mmc init,显示的是mmc  vailable。

谁能帮我解释解释...为什么我在SD模式下,从SD进入uboot状态却不能mmc init...

  • 问题已经解决了...把mmc init 改成输入 mmc rescan 0 就行了。然后fatload mmc 1 81000000 uImage改成fatload mmc 0 81000000 uImage .

  • 您好,我按照您在luhao806的专栏写的DM8168心得之从sd卡烧写到nand 进行nand flash烧写。

    在TI8168_EVM#nand erase 0x0 0x260000;     nand write.i 0x81000000 0x0 0x260000 处都碰到了  no devices available

    请问这是什么问题?

    然后我不管这些继续往下进行,在fatload mmc 0 81000000 rd-jffs2.bin处,有错误:

    reading rd-jffs2.bin                                                            
    Invalid FAT entry                                                               
                                                                                    
    ** Unable to read "rd-jffs2.bin" from mmc 0:1 **

    我将rd-jjfs2.bin,u-boot.noxip.bin,uImage都放在了SD卡的BOOT文件夹,这样对么?

    谢谢~