我用的是闻亭做的DM8168的板子。情况是这样的:
1.SD已经能正常启动,我想从SD烧写到nand,在uboot状态下我输入mmc init,没反应,接下来fatload mmc 1 0x81000000 uImage也是没法执行的。
2.我从nandflash启动到uboot状态,然后出入mmc init,显示的是mmc vailable。
谁能帮我解释解释...为什么我在SD模式下,从SD进入uboot状态却不能mmc init...
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,我按照您在luhao806的专栏写的DM8168心得之从sd卡烧写到nand 进行nand flash烧写。
在TI8168_EVM#nand erase 0x0 0x260000; nand write.i 0x81000000 0x0 0x260000 处都碰到了 no devices available
请问这是什么问题?
然后我不管这些继续往下进行,在fatload mmc 0 81000000 rd-jffs2.bin处,有错误:
reading rd-jffs2.bin
Invalid FAT entry
** Unable to read "rd-jffs2.bin" from mmc 0:1 **
我将rd-jjfs2.bin,u-boot.noxip.bin,uImage都放在了SD卡的BOOT文件夹,这样对么?
谢谢~