This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求教大神关于IBL的program i2cnorboot to NOR



C6657LS、mcsdk_2_01_02_06

今天按照bootloader里面的readme.txt上的说明,把IBL配置好了,已经输出:EEPROM programming completed successfully

而且在Srcipts->EVM c6657 IBL -> setConfig_c6657_main运行了一下也显示成功了。

最后加载NOR 时打印输出NOR programming completed successfully

 

这是不是代表我可以把启动按钮更改为IBL NOR boot on image 0模式然后断电重启EVM查看程序是否在运行?

我尝试把一个在连接状态时运行成功的LED闪烁程序加载到NOR里面,然后配置启动模式断电重启,但是LED并么有闪烁,请问这是为什么?

谢谢

  • 今天重新弄了一遍成功了,但是有一个新问题,当我试图烧写一个6M的程序到NOR时遇到如下问题:

    NOR Writer Utility Version 01.00.00.03

    The data file is too big to fit into the device.

    Error in parsing CCS file app.bin

    查看REFERENCE说的NOR是16MB,但是为什么烧写6M就显示过大呢?

     

    于是我想把这个程序烧写到NAND FLASH里面。

    按照readme操作完成以后,把上面的LED程序烧写到NAND里面,但是无论更改启动方式到IBL NAND boot on image 0还是IBL NAND boot on image 1都无法启动LED闪烁程序,请问这是为什么?我之前已经配置过setConfig_c6657_main()了的。

  • 6657 EVM上的NOR是32Mb(4MB),6678的nand烧写程序用在6657上会有问题,因为NAND的型号不一致

  • 我用的6657的NAND烧写程序哦,后来重新操作了一次成功了。谢谢。