This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6678的SGMII与88E1111之间LINK UP始终不成功!



参考EVM的电路设计,电路上的改动包括下面几个方面

(1)6678两个SGMII接口分别连接88E1111;

(2)SGMII0连接的88E1111的PHY地址配置为“00001”,SGMII1连接的88E1111的PHY地址配置为“00010”;

(3)88E1111的DVDD电压为1.0V,与6678的CVDD1电源相连,88E1111的2.5V等6678的所有电源上电完成后再输出;

6678的上电顺序以及复位时序严格按照推荐的设计;

88E1111的复位时序也严格按照手册推荐的控制;

目前情况是,用PA_simpleExample_exampleProject工程测试,在EVM上可以通过,在我们的板卡上一直在判断LINK UP处循环。

请专家多多指导,谢谢了!