This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6678: TI优化后的线性代数库BLAS——Linalg的例子dgemm编译所遇到的问题

Part Number: TMS320C6678


您好,我想在CCS上运行ti自带的dgemm例子,查询用户手册后,按照用户手册的编译方式进行操作:

1、安装skd,版本是

2、设置环境变量:

3、先编译linarch生成库

4、加上linarch的环境变量,再编译linalg,命令如下:make DSPlibs MEM_MODEL=Medium TARGET=SOC_C6678 LIBOS=LIB_RTOS

生成linalg的库

以上操作都无误。

5、加上linalg的环境变量,编译linalg的example

命令如下:make TARGET=SOC_C6678

结果报如下错误:

我有两个问题:

①请问上面的错误该如何解决呢?

②整个编译过程使用的编译器是ti-cgt-c6000_8.3.2,我尝试着使用7.4版本的编译器,编译linalg库时会造成错误,如for循环中不能定义int、声明数组[]长度不能为0等错误,如何能使用7.4的编译器编译?