This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于DM8148的启动问题



您好:

我们之前用TMS320DMDM8127BCYE3做过一套产品板,通过UART烧写UBOOT.MIN和UBOOT均正常,系统也可以正常运行,这次改板换用了TMS320DM8148CCYE2,通过UART可以下载u-boot.min.uart,但是下载完成后串口就没有反应了。将DM8127板和DM8148板上的FLASH调换,DM8148板的UBOOT、内核和应用程序均可以正常运行,DM8127板也能烧写FLASH,两个板用的DDR和FLASH型号均一样,UBOOT的版本为TI814X-LINUX-PSP-04.01.00.07,请教可能是什么原因导致DM8148的板子通过UART不能烧写呢?谢谢!!另外:两个板子的BTMODE配置也一样。

  • 我尝试了通过SD卡启动,DM8127的板子可以启动,DM8148的板子串口没反应,难道要用仿真器下载调试?

  • 你好!请问你这个问题是怎么解决的?我也有类似情况。我的是自己画的DM8127板,DDR2(MT47H64M16HR)数据线只画了24位,所以我调试的时候是配置成16位模式,uboot.min可以下进去,但是不反馈提示符,您看看可能是什么原因?另外我们还画有一个8127板,只在DDR1接口上接了两片16位DDR2,但是这块板子根本下不进去uboot.min,您知道回事什么原因吗?