Error connecting to the target:
Error 0x80000240/-1180
Fatal Error during: Initialization, OCS,
The target is stuck in Wait-in-Reset mode. The applied reset must be released before progressing.
Board Name: DM6467_xds560
Cpu Name: C6400PLUS_0
Abort: Close Code Composer Studio.
Retry: Try to connect to the target again.
Cancel: Remain disconnected from the target
Diagnostic: Run diagnostic utility.
麻烦帮忙看一下,谢谢~