This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

我的DM6467链接出问题了,ARM能连上,DSP连接不上



Error connecting to the target:
Error 0x80000240/-1180
Fatal Error during: Initialization, OCS,
The target is stuck in Wait-in-Reset mode. The applied reset must be released before progressing.

Board Name: DM6467_xds560
Cpu Name: C6400PLUS_0

Abort: Close Code Composer Studio.
Retry: Try to connect to the target again.
Cancel: Remain disconnected from the target
Diagnostic: Run diagnostic utility.

麻烦帮忙看一下,谢谢~