AM335X通过GPMC和FPGA连接(CPU NMI连接到FPGA IRQ上),FPGA外部管理16个串口中断,当外部设备同时触发中断时,FPGA中断寄存器记录,同时触发CPU让CPU去读取寄存器上的内容。现在有几个问题想问一下
1.AM335X和FPGA中断一根线NMI连接到IRQ上是否合理?因为NMI是固定的中断和异常已经把中断向量表前32个给占了。
2.FPGA中断管理怎么去做?是否通过request_irq去做?如果是,连接串口驱动的方式是否也通过request_irq?
3.CPU分辨哪一路驱动是通过读取FPGA去操作,但是怎样操作相应的串口?
4.16个串口是否应该同时注册一个NMI的中断号?