This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335X FPGA 中断管理



AM335X通过GPMC和FPGA连接(CPU NMI连接到FPGA IRQ上),FPGA外部管理16个串口中断,当外部设备同时触发中断时,FPGA中断寄存器记录,同时触发CPU让CPU去读取寄存器上的内容。现在有几个问题想问一下

1.AM335X和FPGA中断一根线NMI连接到IRQ上是否合理?因为NMI是固定的中断和异常已经把中断向量表前32个给占了。

2.FPGA中断管理怎么去做?是否通过request_irq去做?如果是,连接串口驱动的方式是否也通过request_irq?

3.CPU分辨哪一路驱动是通过读取FPGA去操作,但是怎样操作相应的串口?

4.16个串口是否应该同时注册一个NMI的中断号?

  • 1.AM335X和FPGA中断一根线NMI连接到IRQ上是否合理?因为NMI是固定的中断和异常已经把中断向量表前32个给占了。

       回答:我认为是合理的,因为这个NMI的管脚就是给外部中断使用的

    2.FPGA中断管理怎么去做?是否通过request_irq去做?如果是,连接串口驱动的方式是否也通过request_irq?

       回答:我认为应该用driver层的request_irq()函数去注册中断,nmi中断号为7

    3.CPU分辨哪一路驱动是通过读取FPGA去操作,但是怎样操作相应的串口?

      回答:这个要通过具体驱动程序来控制。

     4.16个串口是否应该同时注册一个NMI的中断号?

       回答:因为16c554是通过FPGA控制的,因此注册一个NMI驱动就可以了

  • 等16port板子回来后再说吧,昨天我们2口的量产了,但是SPIFLASH都没打招呼就换了芯片厂家。驱动改过了,今天早晨已经能够正常运行了。这些小问题就不问你了。等16口的板子出来后就会忙很多,到时候在问吧。

  • SPI FLASH换的谁家的?