This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM385内核运行后无法加载文件系统分区?



DM385 IPNC

通过sd卡启动,运行到加载文件系统那一步程序好像是找不到mmc设备了?请问这是什么情况?

最后卡在 Waiting for root device /dev/mmcblk0p2... ,下面是log信息

 
[BEGIN] 2014/8/27 10:37:20


U-Boot 2010.06-dirty (Aug 27 2014 - 09:38:11) DM385_IPNC_3.50.00

DM385-GP rev 1.1

ARM clk: 600MHz
DDR clk: 533MHz
L3 clk: 200MHz
IVA clk: 450MHz
ISS clk: 400MHz
DSP Default OFF
DSS Default OFF

DRAM:  1 GiB
MMC:   OMAP SD/MMC: 0, ON-BOARD SDIO: 1
Using default environment

The 2nd stage U-Boot will now be auto-loaded
Please do not interrupt the countdown till DM385_IPNC prompt if 2nd stage is already flashed
Hit any key to stop autoboot:  0 
reading u-boot.bin

199440 bytes read
## Starting application at 0x80800000 ...


U-Boot 2010.06-dirty (Aug 27 2014 - 09:39:12) DM385_IPNC_3.50.00

DM385-GP rev 1.1

ARM clk: 600MHz
DDR clk: 533MHz
L3 clk: 200MHz
IVA clk: 450MHz
ISS clk: 400MHz
DSP Default OFF
DSS Default OFF

I2C:   ready
DRAM:  1 GiB
NAND:  HW ECC BCH8 Selected
NAND device: Manufacturer ID: 0xad, Chip ID: 0xda (Hynix NAND 256MiB 3,3V 8-bit)
NAND bus width 16 instead 8 bit
No NAND device found!!!
0 MiB
MMC:   OMAP SD/MMC: 0, ON-BOARD SDIO: 1
@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@
@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@
@@                                                               @@
@@                                                               @@
@@                                                               @@
@@                                                               @@
@@      @@@        @.   @.         @@@@    @@@@  G@@@@@@         @@
@@      @@@@@     L@@  @@@        @@@@@@  @@@@@i @@@@@@          @@
@@      @@ @@@.   @@@  @@@            @@  @,  @@ :@@             @@
@@      @@   @@   @@@  @@@          @@@@  @@;@@: C@@@@@.         @@
@@      @@    @@  @@@.l@L@         G@@@   ,@@@@  @@@  @@         @@
@@      @@    @@ l@ @@@@ @.          l@@  @@ L@@  @   G@         @@
@@      @@    @@ @@ @@@@ @@           @@ C@   @@      @@         @@
@@      @@   ,@C @@ @@@  @@       @i  @@ C@   @@ @@   @@         @@
@@      @@@@@@@  @@  @@  @@       @@@@@l  @@@@@@ L@@@@@          @@
@@       @@@@@   @   @    @        L@@     @@@,   ,@@G           @@
@@                                                               @@
@@                                                               @@
@@                                                               @@
@@                                                               @@
@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@
@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@

Date: 2000-01-01 (Sunday)    Time: 17:59:33
Net:   Ethernet clocking: 0x52
<ethaddr> not set. Reading from E-fuse
Detected MACID:c4:ed:ba:c3:9d:aa
cpsw
Hit any key to stop autoboot:  0 
reading boot.scr

408 bytes read
Running bootscript from MMC/SD to set the ENV...
## Executing script at 80900000
Saving Environment to MMC...
Writing to MMC(0)... done
reading uImage

2481468 bytes read
## Booting kernel from Legacy Image at 80009000 ...
   Image Name:   Linux-2.6.37_DM385_IPNC_3.50.00
   Created:      2014-08-27   2:03:21 UTC
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    2481404 Bytes = 2.4 MiB
   Load Address: 80008000
   Entry Point:  80008000
   Verifying Checksum ... OK
   Loading Kernel Image ... OK
OK

Starting kernel ...

Uncompressing Linux... done, booting the kernel.
Linux version 2.6.37_DM385_IPNC_3.50.00 (root@xubbwd-virtual-machine) (gcc version 4.5.3 20110311 (prerelease) (GCC) ) #1 Wed Aug 27 10:03:17 CST 2014

CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7f

CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache

Machine: dm385ipnc

vram size = 4194304 at 0x0

bootconsole [earlycon0] enabled

ti81xx_reserve: ### Reserved DDR region @84f00000

reserved size = 4194304 at 0x0

FB: Reserving 4194304 bytes SDRAM for VRAM

Memory policy: ECC disabled, Data cache writeback

OMAP chip is DM385 1.0

SRAM: Mapped pa 0x402f1000 to va 0xfe400000 size: 0xf000

Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 19040

Kernel command line: console=ttyO0,115200n8 noinitrd mem=80M rootwait vram=4M notifyk.vpssm3_sva=0xBFD00000 root=/dev/mmcblk0p2 rw eth=00:0C:0C:02:30:FB ip=172.16.0.241 cmemk.phys_start=0x85000000 cmemk.phys_end=0x89000000 cmemk.allowOverlap=1 earlyprintk

cpsw: kernel boot params Ethernet address: 00:0C:0C:02:30:FB

PID hash table entries: 512 (order: -1, 2048 bytes)

Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)

Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)

Memory: 74MB 1MB = 75MB total

Memory: 70676k/70676k available, 11244k reserved, 0K highmem

Virtual kernel memory layout:

    vector  : 0xffff0000 - 0xffff1000   (   4 kB)

    fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)

    DMA     : 0xffc00000 - 0xffe00000   (   2 MB)

    vmalloc : 0xc5800000 - 0xf8000000   ( 808 MB)

    lowmem  : 0xc0000000 - 0xc5000000   (  80 MB)

    pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)

    modules : 0xbf000000 - 0xbfe00000   (  14 MB)

      .init : 0xc0008000 - 0xc003e000   ( 216 kB)

      .text : 0xc003e000 - 0xc04b9000   (4588 kB)

      .data : 0xc04ba000 - 0xc04f9f00   ( 256 kB)

SLUB: Genslabs=11, HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1

NR_IRQS:375

IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts

Total of 128 interrupts on 1 active controller

GPMC revision 6.0

Trying to install interrupt handler for IRQ368

Trying to install interrupt handler for IRQ369

Trying to install interrupt handler for IRQ370

Trying to install interrupt handler for IRQ371

Trying to install interrupt handler for IRQ372

Trying to install interrupt handler for IRQ373

Trying to install interrupt handler for IRQ374

Trying to install type control for IRQ375

Trying to set irq flags for IRQ375

OMAP clockevent source: GPTIMER1 at 20000000 Hz

Console: colour dummy device 80x30

Calibrating delay loop... 599.65 BogoMIPS (lpj=2998272)

pid_max: default: 32768 minimum: 301

Security Framework initialized

Mount-cache hash table entries: 512

CPU: Testing write buffer coherency: ok

devtmpfs: initialized

TI81XX: Map 0x84f00000 to 0xfe500000 for dram barrier

TI81XX: Map 0x40300000 to 0xfe600000 for sram barrier

omap_voltage_early_init: voltage driver support not added

regulator: core version 0.5

regulator: dummy: 

NET: Registered protocol family 16

omap_voltage_domain_lookup: Voltage driver init not yet happened.Faulting!

omap_voltage_add_dev: VDD specified does not exist!

OMAP GPIO hardware version 0.1

OMAP GPIO hardware version 0.1

OMAP GPIO hardware version 0.1

OMAP GPIO hardware version 0.1

omap_mux_init: Add partition: #1: core, flags: 4

Cannot clk_get ck_32

Debugfs: Only enabling/disabling deep sleep and wakeup timer is supported now

registered ti81xx_vpss device

registered ti81xx_vidout device

registered ti81xx on-chip HDMI device

registered ti81xx_fb device

PWM0 init success.

PWM1 init success.

bio: create slab <bio-0> at 0

SCSI subsystem initialized

omap2_mcspi: probe of omap2_mcspi.3 failed with error -2

omap2_mcspi: probe of omap2_mcspi.4 failed with error -2

USBSS revision 4ea2080b

registerd cppi-dma Intr @ IRQ 17

Cppi41 Init Done

omap_i2c omap_i2c.1: bus 1 rev4.0 at 100 kHz

regulator: VRTC: 1800 mV 

regulator: VIO: 1500 mV 

regulator: VDD1: 600 <--> 1500 mV at 1150 mV 

regulator: VDD2: 600 <--> 1500 mV at 1350 mV 

regulator: VDDCTRL: 600 <--> 1400 mV at 1350 mV 

regulator: LDO1: 1100 <--> 3300 mV at 1800 mV 

regulator: LDO2: 1100 <--> 3300 mV at 1800 mV 

regulator: LDO3: 1100 <--> 3300 mV at 3300 mV 

regulator: LDO4: 1100 <--> 3300 mV at 1800 mV 

regulator: LDO5: 1100 <--> 3300 mV at 3300 mV 

regulator: LDO6: 1100 <--> 3300 mV at 3300 mV 

regulator: LDO7: 1100 <--> 3300 mV at 3300 mV 

regulator: LDO8: 1100 <--> 3300 mV at 1800 mV 

tps65911-rtc tps65911-rtc: rtc core: registered tps65911-rtc as rtc0

tps65910 1-002d: No interrupt support, no core IRQ

Advanced Linux Sound Architecture Driver Version 1.0.23.

Switching to clocksource gp timer

musb-hdrc: version 6.0, peripheral, debug=0

musb-hdrc musb-hdrc.0: dma type: dma-cppi41

MUSB controller-0 revision 4ea20800

usb2phy: computed values rxcalib(15)DACs(34 14 15)

usb2phy: override computed values rxcalib(15)DACs(34 14 15)

usb2phy_config: musb(0) rxcalib done, rxcalib read value 6f715d7e

musb-hdrc musb-hdrc.0: USB Peripheral mode controller at c581e000 using DMA, IRQ 18

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 4096 (order: 3, 32768 bytes)

TCP bind hash table entries: 4096 (order: 2, 16384 bytes)

TCP: Hash tables configured (established 4096 bind 4096)

TCP reno registered

UDP hash table entries: 256 (order: 0, 4096 bytes)

UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)

NET: Registered protocol family 1

RPC: Registered udp transport module.

RPC: Registered tcp transport module.

RPC: Registered tcp NFSv4.1 backchannel transport module.

NetWinder Floating Point Emulator V0.97 (double precision)

PMU: registered new PMU device of type 0

omap-iommu omap-iommu.0: ducati registered

omap-iommu omap-iommu.1: sys registered

JFFS2 version 2.2. (NAND) 漏 2001-2006 Red Hat, Inc.

msgmni has been set to 138

io scheduler noop registered

io scheduler deadline registered

io scheduler cfq registered (default)

CMEMK module: built on Aug 26 2014 at 20:51:56

  Reference Linux version 2.6.37

  File /opt/GIT/dm385_viazijing/IPNC_RDK_GA_Release3.5.0/Source/ti_tools/linuxutils_3_23_00_01/packages/ti/sdo/linuxutils/cmem/src/module/cmemk.c

allocated heap buffer 0xc7000000 of size 0x4000000

cmemk initialized

Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled

omap_uart.0: ttyO0 at MMIO 0x48020000 (irq = 72) is a OMAP UART0

console [ttyO0] enabled, bootconsole disabled
console [ttyO0] enabled, bootconsole disabled

omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
brd: module loaded
loop: module loaded
omap2-nand driver initializing
ONFI flash detected
NAND device: Manufacturer ID: 0xad, Chip ID: 0xda (Hynix 																																																																																																										)
Creating 8 MTD partitions on "omap2-nand.0":
0x000000000000-0x000000020000 : "U-Boot-min"
0x000000020000-0x000000260000 : "U-Boot"
0x000000260000-0x000000280000 : "U-Boot Env"
0x000000280000-0x0000006c0000 : "Kernel"
0x0000006c0000-0x000006fc0000 : "File System"
0x000006fc0000-0x000007bc0000 : "Data"
0x000007bc0000-0x00000b0c0000 : "File System2"
0x00000b0c0000-0x000010000000 : "Reserved"
davinci_mdio davinci_mdio.0: davinci mdio revision 1.6
davinci_mdio davinci_mdio.0: detected phy mask fffffffe
davinci_mdio.0: probed
davinci_mdio davinci_mdio.0: phy[0]: device 0:00, driver unknown
mice: PS/2 mouse device common for all mice
i2c /dev entries driver
Linux video capture interface: v2.00
OMAP Watchdog Timer Rev 0x00: initial timeout 60 sec
notify_shm_drv: no DSP present (MULTIPROC_INVALIDID)
notify_init : notify drivercreated  for  remote proc id 1 at physical Address 0xbfd00000
cm: Module associated with clock hdmi_i2s_fck didn't enable in 100000 tries
asoc: tlv320aic3x-hifi <-> davinci-mcasp.1 mapping ok
asoc: HDMI-DAI-CODEC <-> hdmi-dai mapping ok
ALSA device list:
  #0: TI81XX EVM
nf_conntrack version 0.5.0 (1104 buckets, 4416 max)
ip_tables: (C) 2000-2006 Netfilter Core Team
TCP cubic registered
NET: Registered protocol family 17
Bridge firewalling registered
lib80211: common routines for IEEE802.11 drivers
Registering the dns_resolver key type
VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
omap_voltage_late_init: Voltage driver support not added
Power Management for TI81XX.
Detected MACID=0:c:c:2:30:fb
tps65911-rtc tps65911-rtc: setting system clock to 2000-01-01 17:59:42 UTC (946749582)

CPSW phy found : id is : 0x7c0f1
PHY 0:01 not found
IP-Config: Guessing netmask 255.255.0.0
IP-Config: Complete:
     device=eth0, addr=172.16.0.241, mask=255.255.0.0, gw=255.255.255.255,
     host=172.16.0.241, domain=, nis-domain=(none),
     bootserver=255.255.255.255, rootserver=255.255.255.255, rootpath=
Waiting for root device /dev/mmcblk0p2...

[END] 2014/8/27 10:37:58