This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM1802上电电压异常:1.2上电后3.3VIO上有1.3V的电压

Other Parts Discussed in Thread: LM1117

按1802的要求,需要控制上电顺序,先后顺序依次为:1.2V、1.8V、3.3V。

在调试过程中发现当1.2V上电,另两组未上电时,3.3V的电源上有电压,约为1.3V,断开3.3V的供电电源,该电压仍存在,加上1.8V电源(3.3V不加电),3.3V的电源上有1.2V的电压,该电压有非常强的带负载能力。感觉象是1.2V电源串到3.3V电源上了,当加上3.3V电源时,1.2V电源还是1.2V,说明1.2V电源与3.3V电源是不通的。

拆除板上除DDR2外的所有有源器件,仍是上面结果。

不知道是1802本身就是样,还是我的设计有问题导致的。麻烦帮我澄清一下。谢谢!

附件是最小系统原理图,非常感谢!

AM1802-CPU-SCH.pdf