This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA2SX: A15_0跑NDK,TCP发送大数据会产生固定位置丢包的问题

Part Number: TDA2SX

尊敬的工程师,您好

       我在使用TDA2的以太网功能,原本PROCESS_RADAR_SDK默认NDK是运行在IPU1_1,现在需要使用TCP往PC传输大数据,因此我将NDK定义到了A15_0的内核运行,网络1000Mbps速率协商正常,TCP连接正常,但是发现吞吐率太慢,通过wireShake抓包之后发现,发送4MB的数据时,都会在数据发到90kB到100kB之间产生几帧的连续丢失,造成这几帧不断的re transmission,除了这几帧丢失之外,其余数据发送正常。

      因此我想问一下,将NDK配置到A15_0需要注意什么,有没有配置项目被我遗漏了,针对以上现象我该如何排查?麻烦工程师给我一些指导建议,谢谢!

  • 我主要做了如下修改:

    1、 在tda2xx_cascade_bios_radar 目录下的cfg.mk文件里 设置 NDK_PROC_TO_USE=a15_0 

    2、重新生成usecases里的相关priv.c和priv.h文件,主要是把NetworkTx (IPU1_1)修改为NetworkTx (A15)

    3、在文件mem_segment_definition_bios.xs中适当的调整了增加了NDK_DATA_SIZE 和 A15_0_DATA_SIZE, 具体如下:

    /*
     *  ======== mem_segment_definition.xs ========
     *  ======== Single file for the memory map configuration of all cores =========
     */
    
    function getMemSegmentDefinition_external(core)
    {
        KB=1024;
        MB=KB*KB;
    
        DDR3_ADDR                   = 0x80000000;
        DDR3_SIZE                   = 512*MB;
    
        /*
         * In case of ECC_FFI_INCLUDE, DDR3_BASE_ADDR_1 and DDR3_BASE_SIZE_1
         * are hard-coded in as values of gIpcNonCachedDataAddr and
         * gIpcNonCachedDataSize in Ipu1_0.cfg
         * If this DDR3_BASE_SIZE_0 is changed, update  Ipu1_0.cfg
         */
        DDR3_BASE_ADDR_0            = DDR3_ADDR;
        DDR3_BASE_SIZE_0            = 507*MB;
    
        /* The start address of the second mem section should be 16MB aligned.
         * This alignment is a must as a single 16MB mapping is used for EVE
         * to map SR0, REMOTE_LOG_MEM sections.
         * tlb_config_eveX.c need to be modified otherwise
         */
        DDR3_BASE_ADDR_1            = DDR3_BASE_ADDR_0 + DDR3_BASE_SIZE_0;
        DDR3_BASE_SIZE_1            = DDR3_SIZE - DDR3_BASE_SIZE_0;
        //if(core=="ipu1_1" || core=="ipu1_0" || core=="ipu2" || core=="a15_0")
        //{
            /*  for ipu1_0, ipu1_1, ipu2 DDR3_BASE_ADDR_1 should be
             *  in non-cached virtual address of
             *  DDR3_BASE_ADDR_1 + 512*MB
             */
            DDR3_BASE_ADDR_1        = DDR3_BASE_ADDR_1+512*MB;
        //}
    
        DSP1_L2_SRAM_ADDR           = 0x40800000;
        DSP1_L2_SRAM_SIZE           = 288*KB;
    
        DSP2_L2_SRAM_ADDR           = 0x41000000;
        DSP2_L2_SRAM_SIZE           = 288*KB;
    
        EVE1_SRAM_ADDR              = 0x42000000;
        EVE1_SRAM_SIZE              = 1*MB;
    
        EVE2_SRAM_ADDR              = 0x42100000;
        EVE2_SRAM_SIZE              = 1*MB;
    
        EVE3_SRAM_ADDR              = 0x42200000;
        EVE3_SRAM_SIZE              = 1*MB;
    
        EVE4_SRAM_ADDR              = 0x42300000;
        EVE4_SRAM_SIZE              = 1*MB;
    
        TOTAL_MEM_SIZE              = (DDR3_SIZE);
    
        /* First 512 MB - cached */
        /* EVE vecs space should be align with 16MB boundary, and if possible try to fit
         * the entire vecs+code+data in 16MB section. In this case a single TLB map would
         * be enough to map vecs+code+data of an EVE.
         * tlb_config_eveX.c need to be modified if any of these EVE memory sections or
         * SR1_FRAME_BUFFER_MEM section is modified.
         */
    
        /* EVE self-branch instruction block - EVE1_VECS
         * In SBL, EVE self-branch instruction is inserted @ 0x80000000 if no AppImage for EVE.
         * This could overwrites the code/data loaded at 0x80000000.
         * So Reserving a small memory block in the beginning of the DDR @0x8000 0000 for
         * EVE self-branch instruction if no AppImage for EVE.
         * If EVE enabled, then the EVE VECS/DATA/CODE is placed @0x8000 0000,
         * and hence we did not observe any issue.
         * If EVE is disabled, then also DO NOT remove this EVE1_VECS section @0x80000000,
         * if no AppImage for EVE. This could overwrites the code/data loaded at 0x80000000
         */
    
        EVE1_VECS_SIZE              = 0.5*MB;
        EVE1_CODE_SIZE              =   2*MB;
        EVE1_DATA_SIZE              =13.5*MB;
        EVE2_VECS_SIZE              = 0.5*MB;
        EVE2_CODE_SIZE              =   2*MB;
        EVE2_DATA_SIZE              =13.5*MB;
        EVE3_VECS_SIZE              = 0.5*MB;
        EVE3_CODE_SIZE              =   2*MB;
        EVE3_DATA_SIZE              =13.5*MB;
        EVE4_VECS_SIZE              = 0.5*MB;
        EVE4_CODE_SIZE              =   2*MB;
        EVE4_DATA_SIZE              =13.5*MB;
        NDK_DATA_SIZE               =   8*MB;
        
        if(java.lang.System.getenv("ECC_FFI_INCLUDE")=="yes")
        {
            IPU1_1_CODE_SIZE            = 2.5*MB;
            IPU1_1_DATA_SIZE            = 12.5*MB;
            IPU1_0_CODE_SIZE            =  6*MB;
            IPU1_0_DATA_SIZE            =  12*MB;
        }
        else
        {
            IPU1_1_CODE_SIZE            = 2.5*MB;
            IPU1_1_DATA_SIZE            = 12.5*MB;
            IPU1_0_CODE_SIZE            =  6*MB;
            IPU1_0_DATA_SIZE            =  16*MB;
        }
        IPU2_CODE_SIZE              =   2*MB;
        IPU2_DATA_SIZE              =   7*MB;
        DSP1_CODE_SIZE              =   6*MB;
        DSP1_DATA_SIZE              =  14*MB;
        DSP1_DATA_SIZE_2            =   1*MB;
        DSP2_CODE_SIZE              =   4*MB;
        DSP2_DATA_SIZE              =  14*MB;
        DSP2_DATA_SIZE_2            =   1*MB;
        /* A15_0_CODE_SIZE reduced since it is not used in .bld file.
         * Check .bld for details. Originally 2 + 14 MB.
         */
        A15_0_DATA_SIZE             =  43.5*MB;
        if(java.lang.System.getenv("OPENCL_INCLUDE") == "yes")
        {
            A15_0_DATA_SIZE_INC     =  101*MB /* in MB */
            A15_0_DATA_SIZE         =  (A15_0_DATA_SIZE + A15_0_DATA_SIZE_INC);
        }
    
        if(java.lang.System.getenv("ECC_FFI_INCLUDE")=="yes")
        {
            /* Ensure ECC regions are 64kB aligned */
            SR1_FRAME_BUFFER_SIZE       = 297.5*MB;
            SR1_BUFF_ECC_ASIL_SIZE      =   1*MB;
            SR1_BUFF_ECC_QM_SIZE        =  40*MB;
            SR1_BUFF_NON_ECC_ASIL_SIZE  =   1*MB;
        }
        else
        {
            SR1_BUFF_ECC_ASIL_SIZE      =   4*KB;
            SR1_BUFF_ECC_QM_SIZE        =   4*KB;
            SR1_BUFF_NON_ECC_ASIL_SIZE  =   4*KB;
            SR1_FRAME_BUFFER_SIZE       = 305.5*MB - (SR1_BUFF_ECC_ASIL_SIZE + SR1_BUFF_ECC_QM_SIZE + SR1_BUFF_NON_ECC_ASIL_SIZE);
            if(java.lang.System.getenv("OPENCL_INCLUDE") == "yes")
            {
                SR1_FRAME_BUFFER_SIZE   = SR1_FRAME_BUFFER_SIZE - A15_0_DATA_SIZE_INC;
            }
        }
    
        /* Second 512 MB - non-cached */
        /* The start address of the second mem section should be 16MB aligned.
         * This alignment is a must as a single 16MB mapping is used for EVE
         * to map SR0, REMOTE_LOG_MEM sections.
         * tlb_config_eveX.c need to be modified otherwise
         */
        REMOTE_LOG_SIZE             =  160*KB;
        SYSTEM_IPC_SHM_SIZE         =  480*KB;
        SYSTEM_AUTOSAR_IPC_SHM_SIZE =  512*KB;
        LINK_STATS_SIZE             =  256*KB;
        HDVPSS_DESC_SIZE            = 1024*KB;
        SR0_SIZE                    =  128*KB;
        OPENVX_SHM_SIZE             = 1984*KB;
        EEPROM_PARAM_SIZE           =   64*KB;
    
        if((java.lang.System.getenv("OPENCL_INCLUDE") == "yes"))
        {
            /* when OpenCL is enabled we need more SR0 space
             */
            SR0_SIZE                =  2*MB;
        }
    

    4、使用MAC0 ,并设置了静态IP;

    现象描述:如果NDK配置在IPU1_1中运行,千兆网络通信正常,每帧1MB数据,连续发送,并不会出现丢帧现象;

    但是如果通过以上配置,将NDK配置在A15内核中运行,千兆网络能够正常连接,但是比如连续发送4帧,每帧1MB的数据,

    每次都会在发送第一帧1MB处的90kB-100kB之间出现丢帧,所丢的这些帧通过TCP底层的重发机制最后也都能重发成功,但是这样会导致吞吐率下降,

    由于在IPU1_1中运行正常,在A15中才会出现此现象,因此我感觉是程序里哪儿配置不对,麻烦工程师给指导一下,谢谢。

    wireshake抓包信息如下:

    其中192.168.31.100是PC机。

  • 我们稍后会将您的帖子升级到E2E,会有产品线专家给您提供支持。

  • 您好,产品线专家有回复吗?

  • 您好,暂时还没有,我们来催促一下,英文论坛的链接也给您贴在下面:

    e2e.ti.com/.../tda2sx-tcp-sending-large-data-can-cause-packet-loss-at-a-fixed-location

  • 您好, 我这边测试, 有点进展, 描述如下:

    1) 原本我是在networkTxLink_tsk .c文件里的NetworkTxLink_tskMain函数里进行数据发送,发送代码如下

                               UInt8* chBuf[2];
                                for(c=0;c<2;c++)
                                {
                                    chBuf[0] = (UInt8*)((uint32_t*)(pADCFrames->bufferList.buffers[pADCFrames->rIndex+c*2]->payload))[0];
                                    chBuf[1] = (UInt8*)((uint32_t*)(pADCFrames->bufferList.buffers[pADCFrames->rIndex+c*2+1]->payload))[0];
                                    for(i=0; i<256; i++)
                                    {
                                        TcpSendToAll(chBuf[0], 4096);
                                        TcpSendToAll(chBuf[1], 4096);
                                        chBuf[0] += 4096;
                                        chBuf[1] += 4096;
                                    }
                                }
    上述代码总共发送4MByte的数据,会产生丢帧的问题;
    2)如果在发送的代码里加入Task_sleep进行间歇性的任务休眠,则不会产生丢帧问题
                               UInt8* chBuf[2];
                                for(c=0;c<2;c++)
                                {
                                    chBuf[0] = (UInt8*)((uint32_t*)(pADCFrames->bufferList.buffers[pADCFrames->rIndex+c*2]->payload))[0];
                                    chBuf[1] = (UInt8*)((uint32_t*)(pADCFrames->bufferList.buffers[pADCFrames->rIndex+c*2+1]->payload))[0];
                                    for(i=0; i<256; i++)
                                    {
                                        TcpSendToAll(chBuf[0], 4096);
                                        TcpSendToAll(chBuf[1], 4096);
                                        chBuf[0] += 4096;
                                        chBuf[1] += 4096;
                                        Task_sleep(1);
                                    }
                                }
    我调整休眠间隔,比如发送2次4096字节,在休眠1ms,不丢帧,但是传输速率比较慢;  如果修改为连续发送8次, 4096字节,再休眠1ms, 速率可以提高
    到160Mbps.
     
    我尝试了降低networkTxLink_tsk任务的优先级, 增加TCP的TX缓存, 没有解决问题, 只有加入Task_sleep 才会避免丢包的问题,以及吞吐率才能得到提升;
    麻烦工程师帮忙分析一下改问题, 如何能不加入Task_sleep代码, 还能避免丢包提高吞吐率?
  • 好的我们跟进给工程师了。

  • 您好, 问题有反馈吗?

  • 抱歉暂时还没有,我们催促下工程师看看。