This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教下DM8168的AVS电压,可以使用固定的1.05v供电么,如果没有功耗要求的话

Other Parts Discussed in Thread: TPS40041

如标题,并且电源的设计余量足够,芯片散热也没有问题的前提下。

甚至是否可以把CVDD和CVDDC电源共用

  • 不行, 这路电源必须保证使用调压AVS,这个在DM8168手册里面有要求的。

    http://processors.wiki.ti.com/index.php/DM816x_Design_Resources#Requirements

    AVS is required for DM816x devices. Using a fixed supply voltage level will violate max/min operating conditions for some devices which may fall at the edges of the process corners. This will in turn lead to long term reliability issues and may cause complete device failure.

  • 另外补充下,我看demo板的avs硬件电路,主要就是四个gpio调节TPS40041的电压,另外还有一个msp430单片机检测8168多路电源的各自电流,

    我们做的板子,TPS40041及GPIO这块和demo板一致,把单片机砍掉了,是否影响AVS的工作,或是说AVS模块包括外围的电流检测电路不?

    谢谢盼回复

  • 不会影响AVS工作的,TPS40041配GIPO电阻网络即可。

  • 如果只是进行AVS电压控制,不进行电流检测,是否会影响AVS工作使用呢?我看EVM板是要进行电流监测的;

    是否可以理解:AVS控制只是A8进行电压控制就好,如果没有监测反馈也是能够正常使用的。