使用ccs进行仿真LOAD PROGRAM时报错
错误代码如下:
Trouble Writing Register:
Error 0x80001024/-1058
Fatal Error during: Register, Execution, Target,
Device driver: Emulator Controller not responding
It is recommended to RESET EMULATOR. This will disconnect each
target from the emulator. The targets should then be power cycled
or hard reset followed by an emureset and reconnect to each target.
查了4天,非常着急。可以确认硬件正常、仿真器正常。使用FPGA向DSP发送RST和时钟信号。
请问这种情况是什么问题,DSP芯片能进行正常仿真,需要怎样的控制信号才能保证正常稳定。