This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

5410a芯片CCS仿真程序报错



使用ccs进行仿真LOAD PROGRAM时报错

错误代码如下:

Trouble Writing Register:

Error 0x80001024/-1058

Fatal Error during: Register, Execution, Target,

Device driver: Emulator Controller not responding

It is recommended to RESET EMULATOR.  This will disconnect each

target from the emulator.  The targets should then be power cycled

or hard reset followed by an emureset and reconnect to each target.

查了4天,非常着急。可以确认硬件正常、仿真器正常。使用FPGA向DSP发送RST和时钟信号。

请问这种情况是什么问题,DSP芯片能进行正常仿真,需要怎样的控制信号才能保证正常稳定。