This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教Tony Tang有关EDMA配置问题



Tony Tang

              你好。下面是我配置的EDMA配置,现在是16bit  I2S 数据格式,目前经过测试,没有什么问题。但是我要是把 I2S 数据格式改成24bit ,DMA传输出错,MCASP 状态寄存器显示 Receive DMA error did occur。搞不球明白,特向你请教,谢谢,以下是配置代码

/*
** Default paRAM for Receive section.
*/
static struct EDMA3CCPaRAMEntry const rxDefaultPar =
{
(unsigned int)(EDMA3CC_OPT_SAM | (0x02 << 8u)), /* Opt field */
(unsigned int)SOC_MCASP_0_DATA_REGS, /* source address */
(unsigned short)(4), /* aCnt */
(unsigned short)(256), /* bCnt */
(unsigned int)rxBuf0, /* dest address */
(short) (0), /* source bIdx 0 */
(short)(4), /* dest bIdx */
(unsigned short)(PAR_RX_START * SIZE_PARAMSET), /* link address */
(unsigned short)(0), /* bCnt reload value */
(short)(0), /* source cIdx */
(short)(0), /* dest cIdx */
(unsigned short)1 /* cCnt */
};