各位大牛,这边有两个问题请教下各位:
1、我这边在使用EMAC启动时候无法从网络启动,使用的网络芯片是TLK105,为MII模式,晶振25MHZ,cpu芯片AM3352,cpu晶振24MHz,串口打印信息如下:
U-Boot SPL 2013.01.01 (Sep 29 2014 - 10:41:06)
Could not probe the EEPROM; something fundamentally wrong on the I2C bus.
Could not get board ID.
musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
USB Peripheral mode controller at 47401000 using PIO, IRQ 0
musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
USB Host mode controller at 47401800 using PIO, IRQ 0
Using default environment
<ethaddr> not set. Validating first E-fuse MAC
PHY reset timed out
cpsw
link up on port 0, speed 1000, full duplex
BOOTP broadcast 1
BOOTP broadcast 2
BOOTP broadcast 3
BOOTP broadcast 4
BOOTP broadcast 5
BOOTP broadcast 6
BOOTP broadcast 7
BOOTP broadcast 8
BOOTP broadcast 9
BOOTP broadcast 10
Retry count exceeded; starting again
link up on port 0, speed 1000, full duplex
BOOTP broadcast 1
BOOTP broadcast 2
BOOTP broadcast 3
BOOTP broadcast 4
BOOTP broadcast 5
BOOTP broadcast 6
BOOTP broadcast 7
BOOTP broadcast 8
BOOTP broadcast 9
BOOTP broadcast 10
Retry count exceeded; starting again
link up on port 0, speed 1000, full duplex
BOOTP broadcast 1
2、我另一个板子使用的是USB启动,这个可以正常启动kernel并且也可以把内核和文件系统烧录到eMMC,但是调试网络部分的时候,能够识别到TLK105的百兆网,但是无法获取ip,打印如下:
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
[ 0.000000] Linux version 3.2.0 (zhyf@ECU-SERVER) (gcc version 4.7.3 20130226
(prerelease) (crosstool-NG linaro-1.13.1-4.7-2013.03-20130313 - Linaro GCC 2013
.03) ) #4 Fri Oct 31 09:07:27 CST 2014
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instructio
n cache
[ 0.000000] Machine: am335xevm
[ 0.000000] Memory policy: ECC disabled, Data cache writeback
[ 0.000000] AM335X ES2.1 (neon )
[ 0.000000] ------------[ cut here ]------------
[ 0.000000] WARNING: at arch/arm/mach-omap2/clkt_clksel.c:194 omap2_clksel_re
calc+0xc8/0x134()
[ 0.000000] clock: Could not find fieldval 0 for clock dpll_core_m6_ck parent
dpll_core_x2_ck
[ 0.000000] Modules linked in:
[ 0.000000] Backtrace:
[ 0.000000] [<c0017dbc>] (dump_backtrace+0x0/0x10c) from [<c04131e0>] (dump_s
tack+0x18/0x1c)
[ 0.000000] r6:c0030b28 r5:00000009 r4:c05d3e78 r3:c05f450c
[ 0.000000] [<c04131c8>] (dump_stack+0x0/0x1c) from [<c003e2ec>] (warn_slowpa
th_common+0x54/0x6c)
[ 0.000000] [<c003e298>] (warn_slowpath_common+0x0/0x6c) from [<c003e3a8>] (w
arn_slowpath_fmt+0x38/0x40)
[ 0.000000] r8:80000200 r7:c06504a4 r6:00000000 r5:c05e6c38 r4:00000000
[ 0.000000] r3:00000009
[ 0.000000] [<c003e370>] (warn_slowpath_fmt+0x0/0x40) from [<c0030b28>] (omap
2_clksel_recalc+0xc8/0x134)
[ 0.000000] r3:00000000 r2:c0500fe8
[ 0.000000] [<c0030a60>] (omap2_clksel_recalc+0x0/0x134) from [<c003487c>] (p
ropagate_rate+0x34/0x54)
[ 0.000000] r6:c06504dc r5:c05e6b38 r4:c05e6c38
[ 0.000000] [<c0034848>] (propagate_rate+0x0/0x54) from [<c0034888>] (propaga
te_rate+0x40/0x54)
[ 0.000000] r5:c05e6adc r4:c05e6b24
[ 0.000000] [<c0034848>] (propagate_rate+0x0/0x54) from [<c0034888>] (propaga
te_rate+0x40/0x54)
[ 0.000000] r5:c05e6a24 r4:c05e6ac8
[ 0.000000] [<c0034848>] (propagate_rate+0x0/0x54) from [<c0034888>] (propaga
te_rate+0x40/0x54)
[ 0.000000] r5:c05e6910 r4:c05e6a10
[ 0.000000] [<c0034848>] (propagate_rate+0x0/0x54) from [<c00349ec>] (recalcu
late_root_clocks+0x40/0x58)
[ 0.000000] r5:c05f3c6c r4:c05e68fc
[ 0.000000] [<c00349ac>] (recalculate_root_clocks+0x0/0x58) from [<c05a3bd8>]
(am33xx_clk_init+0x84/0xa0)
[ 0.000000] r5:c05e678c r4:c05e678c
[ 0.000000] [<c05a3b54>] (am33xx_clk_init+0x0/0xa0) from [<c05a3920>] (omap3x
xx_clk_init+0xe0/0x314)
[ 0.000000] r5:c086a840 r4:00003517
[ 0.000000] [<c05a3840>] (omap3xxx_clk_init+0x0/0x314) from [<c059d5b8>] (am3
3xx_init_early+0x3c/0x40)
[ 0.000000] r7:c06504a4 r6:c06504dc r5:c086a840 r4:c05c3464
[ 0.000000] [<c059d57c>] (am33xx_init_early+0x0/0x40) from [<c0599de0>] (setu
p_arch+0x714/0x804)
[ 0.000000] [<c05996cc>] (setup_arch+0x0/0x804) from [<c05965a4>] (start_kern
el+0x78/0x2dc)
[ 0.000000] [<c059652c>] (start_kernel+0x0/0x2dc) from [<80008040>] (0x800080
40)
[ 0.000000] r6:c05c48e0 r5:c05d4084 r4:10c53c7d
[ 0.000000] ---[ end trace 1b75b31a2719ed1c ]---
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pag
es: 65024
[ 0.000000] Kernel command line: console=ttyO0,115200n8 root=/dev/mmcblk0p2 r
o rootfstype=ext3 rootwait ip=none
[ 0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
[ 0.000000] Memory: 256MB = 256MB total
[ 0.000000] Memory: 253288k/253288k available, 8856k reserved, 0K highmem
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
[ 0.000000] vmalloc : 0xd0800000 - 0xff000000 ( 744 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xd0000000 ( 256 MB)
[ 0.000000] modules : 0xbf000000 - 0xc0000000 ( 16 MB)
[ 0.000000] .text : 0xc0008000 - 0xc0596000 (5688 kB)
[ 0.000000] .init : 0xc0596000 - 0xc05d1000 ( 236 kB)
[ 0.000000] .data : 0xc05d2000 - 0xc063aa30 ( 419 kB)
[ 0.000000] .bss : 0xc063aa54 - 0xc0669824 ( 188 kB)
[ 0.000000] NR_IRQS:396
[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrup
ts
[ 0.000000] Total of 128 interrupts on 1 active controller
[ 0.000000] OMAP clockevent source: GPTIMER2 at 24000000 Hz
[ 0.000000] OMAP clocksource: GPTIMER1 at 32768 Hz
[ 0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 13
1071999ms
[ 0.000000] Console: colour dummy device 80x30
[ 0.000335] Calibrating delay loop... 298.59 BogoMIPS (lpj=1492992)
[ 0.067657] pid_max: default: 32768 minimum: 301
[ 0.067932] Security Framework initialized
[ 0.068115] Mount-cache hash table entries: 512
[ 0.068847] CPU: Testing write buffer coherency: ok
[ 0.096466] omap_hwmod: gfx: failed to hardreset
[ 0.116577] omap_hwmod: pruss: failed to hardreset
[ 0.118804] print_constraints: dummy:
[ 0.119567] NET: Registered protocol family 16
[ 0.124053] OMAP GPIO hardware version 0.1
[ 0.129913] omap_mux_init: Add partition: #1: core, flags: 0
[ 0.134094] omap_i2c.1: alias fck already exists
[ 0.135925] omap2_mcspi.1: alias fck already exists
[ 0.136444] omap2_mcspi.2: alias fck already exists
[ 0.138610] edma.0: alias fck already exists
[ 0.138671] edma.0: alias fck already exists
[ 0.138702] edma.0: alias fck already exists
[ 0.200408] bio: create slab <bio-0> at 0
[ 0.205230] SCSI subsystem initialized
[ 0.208801] usbcore: registered new interface driver usbfs
[ 0.209503] usbcore: registered new interface driver hub
[ 0.209930] usbcore: registered new device driver usb
[ 0.210540] registerd cppi-dma Intr @ IRQ 17
[ 0.210571] Cppi41 Init Done Qmgr-base(d087a000) dma-base(d0878000)
[ 0.210571] Cppi41 Init Done
[ 0.210632] musb-ti81xx musb-ti81xx: musb0, board_mode=0x13, plat_mode=0x3
[ 0.211242] musb-ti81xx musb-ti81xx: musb1, board_mode=0x13, plat_mode=0x1
[ 0.213714] omap_i2c omap_i2c.1: bus 1 rev2.4.0 at 100 kHz
[ 0.216735] tps65910 1-002d: could not be detected
[ 0.219757] Advanced Linux Sound Architecture Driver Version 1.0.24.
[ 0.222137] Switching to clocksource gp timer
[ 0.257781] musb-hdrc: version 6.0, ?dma?, otg (peripheral+host)
[ 0.258117] musb-hdrc musb-hdrc.0: dma type: dma-cppi41
[ 0.258789] MUSB0 controller's USBSS revision = 4ea20800
[ 0.258850] musb0: Enabled SW babble control
[ 0.260894] musb-hdrc musb-hdrc.0: USB OTG mode controller at d083c000 using
DMA, IRQ 18
[ 0.261199] musb-hdrc musb-hdrc.1: dma type: dma-cppi41
[ 0.261871] MUSB1 controller's USBSS revision = 4ea20800
[ 0.261932] musb1: Enabled SW babble control
[ 0.263000] musb-hdrc musb-hdrc.1: MUSB HDRC host driver
[ 0.263183] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus numbe
r 1
[ 0.263427] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[ 0.263458] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=
1
[ 0.263488] usb usb1: Product: MUSB HDRC host driver
[ 0.263488] usb usb1: Manufacturer: Linux 3.2.0 musb-hcd
[ 0.263519] usb usb1: SerialNumber: musb-hdrc.1
[ 0.265380] hub 1-0:1.0: USB hub found
[ 0.265441] hub 1-0:1.0: 1 port detected
[ 0.266693] musb-hdrc musb-hdrc.1: USB Host mode controller at d083e800 using
DMA, IRQ 19
[ 0.267547] NET: Registered protocol family 2
[ 0.267913] IP route cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.268493] TCP established hash table entries: 8192 (order: 4, 65536 bytes)
[ 0.268859] TCP bind hash table entries: 8192 (order: 3, 32768 bytes)
[ 0.269104] TCP: Hash tables configured (established 8192 bind 8192)
[ 0.269134] TCP reno registered
[ 0.269134] UDP hash table entries: 256 (order: 0, 4096 bytes)
[ 0.269195] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[ 0.269653] NET: Registered protocol family 1
[ 0.270141] RPC: Registered named UNIX socket transport module.
[ 0.270172] RPC: Registered udp transport module.
[ 0.270202] RPC: Registered tcp transport module.
[ 0.270233] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.270690] NetWinder Floating Point Emulator V0.97 (double precision)
[ 0.290710] VFS: Disk quotas dquot_6.5.2
[ 0.290863] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 0.291992] msgmni has been set to 494
[ 0.298583] alg: No test for stdrng (krng)
[ 0.299896] io scheduler noop registered
[ 0.299926] io scheduler deadline registered
[ 0.300079] io scheduler cfq registered (default)
[ 0.302276] Could not set LED4 to fully on
[ 0.305511] omap_uart.0: ttyO0 at MMIO 0x44e09000 (irq = 72) is a OMAP UART0
[ 1.130126] console [ttyO0] enabled
[ 1.135284] omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
[ 1.143768] omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
[ 1.152099] omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3
[ 1.160552] omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4
[ 1.168945] omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5
[ 1.178314] omap4_rng omap4_rng: OMAP4 Random Number Generator ver. 2.00
[ 1.206665] brd: module loaded
[ 1.221221] loop: module loaded
[ 1.225006] i2c-core: driver [tsl2550] using legacy suspend method
[ 1.231567] i2c-core: driver [tsl2550] using legacy resume method
[ 1.238220] at24 1-0051: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[ 1.302825] No daughter card found
[ 1.306549] at24 1-0050: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[ 1.372833] The board is a AM335x Starter Kit.
[ 1.379028] omap_hsmmc.0: alias fck already exists
[ 1.384948] omap_hsmmc.1: alias fck already exists
[ 1.392120] _regulator_get: l3_main.0 supply vdd_core not found, using dummy
regulator
[ 1.400695] am335x_opp_update: physical regulator not present for core(-22)
[ 1.408752] registered am33xx_sr device
[ 1.416748] mtdoops: mtd device (mtddev=name/number) must be supplied
[ 1.424468] omap2-nand driver initializing
[ 1.429199] OneNAND driver initializing
[ 1.436096] CAN device driver interface
[ 1.440185] CAN bus driver for Bosch D_CAN controller 1.0
[ 1.492919] davinci_mdio davinci_mdio.0: davinci mdio revision 1.6
[ 1.499481] davinci_mdio davinci_mdio.0: detected phy mask fffffffd
[ 1.507232] davinci_mdio.0: probed
[ 1.510864] davinci_mdio davinci_mdio.0: phy[1]: device 0:01, driver unknown
[ 1.519104] usbcore: registered new interface driver zd1201
[ 1.525482] usbcore: registered new interface driver cdc_ether
[ 1.532043] usbcore: registered new interface driver cdc_eem
[ 1.538452] usbcore: registered new interface driver dm9601
[ 1.544494] cdc_ncm: 04-Aug-2011
[ 1.548278] usbcore: registered new interface driver cdc_ncm
[ 1.554321] Initializing USB Mass Storage driver...
[ 1.559967] usbcore: registered new interface driver usb-storage
[ 1.566406] USB Mass Storage support registered.
[ 1.572265] mousedev: PS/2 mouse device common for all mice
[ 1.580444] omap_rtc am33xx-rtc: rtc core: registered am33xx-rtc as rtc0
[ 1.588165] i2c /dev entries driver
[ 1.592712] Linux video capture interface: v2.00
[ 1.598358] usbcore: registered new interface driver uvcvideo
[ 1.604522] USB Video Class driver (1.1.1)
[ 1.611877] OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ 1.618835] _regulator_get: deviceless supply vdd_mpu not found, using dummy
regulator
[ 1.628173] cpuidle: using governor ladder
[ 1.633728] cpuidle: using governor menu
[ 1.643463] omap4_aes_mod_init: loading AM33X AES driver
[ 1.649291] omap4-aes omap4-aes: AM33X AES hw accel rev: 3.02
[ 1.656738] omap4_aes_probe: probe() done
[ 1.661468] omap4_sham_mod_init: loading AM33X SHA/MD5 driver
[ 1.667877] omap4-sham omap4-sham: AM33X SHA/MD5 hw accel rev: 4.03
[ 1.692565] omap4_sham_probe: probe() done
[ 1.702484] usbcore: registered new interface driver usbhid
[ 1.708465] usbhid: USB HID core driver
[ 1.714385] usbcore: registered new interface driver snd-usb-audio
[ 1.724761] ALSA device list:
[ 1.727905] No soundcards found.
[ 1.731536] oprofile: hardware counters not available
[ 1.736999] oprofile: using timer interrupt.
[ 1.741577] nf_conntrack version 0.5.0 (3957 buckets, 15828 max)
[ 1.748931] ip_tables: (C) 2000-2006 Netfilter Core Team
[ 1.754852] TCP cubic registered
[ 1.758300] NET: Registered protocol family 17
[ 1.763092] can: controller area network core (rev 20090105 abi 8)
[ 1.769836] NET: Registered protocol family 29
[ 1.774597] can: raw protocol (rev 20090105)
[ 1.779113] can: broadcast manager protocol (rev 20090105 t)
[ 1.785217] Registering the dns_resolver key type
[ 1.790344] VFP support v0.3: implementor 41 architecture 3 part 30 variant c
rev 3
[ 1.798553] ThumbEE CPU extension supported.
[ 1.803222] mux: Failed to setup hwmod io irq -22
[ 1.809570] Power Management for AM33XX family
[ 1.814697] Trying to load am335x-pm-firmware.bin (60 secs timeout)
[ 1.821594] Copied the M3 firmware to UMEM
[ 1.826141] Cortex M3 Firmware Version = 0x181
[ 1.831237] _regulator_get: deviceless supply vdd_core not found, using dummy
regulator
[ 1.839904] smartreflex smartreflex: am33xx_sr_probe: cannot determine opp
[ 1.847259] smartreflex: probe of smartreflex failed with error -22
[ 1.854949] sr_init: platform driver register failed
[ 1.867279] clock: disabling unused clocks to save power
[ 1.889434] mmc1: new high speed MMC card at address 0001
[ 1.896942] mmcblk0: mmc1:0001 P1XXXX 3.60 GiB
[ 1.902313] mmcblk0boot0: mmc1:0001 P1XXXX partition 1 16.0 MiB
[ 1.908966] mmcblk0boot1: mmc1:0001 P1XXXX partition 2 16.0 MiB
[ 1.918640] mmcblk0: p1 p2
[ 1.927581] mmcblk0boot1: unknown partition table
[ 1.936645] mmcblk0boot0: unknown partition table
[ 1.950836] Detected MACID=d0:ff:50:b1:33:91
[ 1.957611] cpsw: Detected MACID = d0:ff:50:b1:33:93
[ 1.965087] omap_rtc am33xx-rtc: setting system clock to 2000-01-01 00:00:00
UTC (946684800)
[ 1.979248] EXT3-fs (mmcblk0p2): recovery required on readonly filesystem
[ 1.986541] EXT3-fs (mmcblk0p2): write access will be enabled during recovery
[ 2.384277] kjournald starting. Commit interval 5 seconds
[ 2.390258] EXT3-fs (mmcblk0p2): recovery complete
[ 2.399475] EXT3-fs (mmcblk0p2): mounted filesystem with ordered data mode
[ 2.406921] VFS: Mounted root (ext3 filesystem) readonly on device 179:2.
[ 2.415161] Freeing init memory: 236K
INIT: version 2.88 booting
Error opening /dev/fb0: No such device
Starting udev
Starting Bootlog daemon: bootlogd: cannot allocate pseudo tty: No such file or d
irectory
bootlogd.
[ 8.546875] EXT3-fs (mmcblk0p2): using internal journal
ALSA: Restoring mixer settings...
/usr/sbin/alsactl: load_state:1686: No soundcards found...
Configuring network interfaces... [ 9.592834] PHY 0:00 not found
udhcpc (v1.20.2) started
Sending discover...
Sending discover...
Sending discover...
No lease, failing
done.
Tue Jun 25 23:08:00 UTC 2013
INIT: Entering runlevel: 5
Starting system message bus: dbus.
Starting telnet daemon.
Starting syslogd/klogd: done
Starting thttpd.
Stopping Bootlog daemon: bootlogd.
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project http://arago-project.org am335x-evm ttyO0
Arago 2013.05 am335x-evm ttyO0
am335x-evm login: root
root@am335x-evm:~# udhcpc -i eth1
udhcpc (v1.20.2) started
[ 29.021118] net eth1: CPSW phy found : id is : 0x2000a211
Sending discover...
[ 31.015197] PHY: 0:01 - Link is Up - 100/Full
Sending discover...
Sending discover...
Sending discover...
还请各位大牛帮帮忙指点一下!不胜感激!!!