This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请教一下,CCS3.3环境下C6743 Boot方式选择 SPI外接的Flash,有没有相关例程???????还不太明白Boot的过程
您好,我在运行烧写程序是程序运行着突然跳到disassembly 窗口:
6088FE40 FFFFFFFF || .word 0xffffffff
6088FE44 FFFFFFFF || .word 0xffffffff
6088FE48 FFFFFFFF || .word 0xffffffff
6088FE4C FFFFFFFF || .word 0xffffffff
6088FE50 FFFFFFFF || .word 0xffffffff
6088FE54 FFFFFFFF || .word 0xffffffff
6088FE58 FFFFFFFF || .word 0xffffffff
6088FE5C FFFFFFFF || .word 0xffffffff
6088FE60 FFFFFFFF || .word 0xffffffff
6088FE64 FFFFFFFF || .word 0xffffffff
6088FE68 FFFFFFFF || .word 0xffffffff
6088FE6C FFFFFFFF || .word 0xffffffff
6088FE70 FFFFFFFF || .word 0xffffffff
6088FE74 FFFFFFFF || .word 0xffffffff
6088FE78 FFFFFFFF || .word 0xffffffff
6088FE7C FFFFFFFF || .word 0xffffffff
6088FE80 FFFFFFFF || .word 0xffffffff
6088FE84 FFFFFFFF || .word 0xffffffff
6088FE88 FFFFFFFF || .word 0xffffffff
6088FE8C FFFFFFFF || .word 0xffffffff
您好,我烧写程序运行不到fp = fopen(“11.bin”,"rb")直接跳到一下Disassembly窗口,请问是什么原因????
B7514DA0 00000000 NOP
B7514DA4 00000000 NOP
B7514DA8 00000000 NOP
B7514DAC 00000000 NOP
B7514DB0 00000000 NOP
B7514DB4 00000000 NOP
B7514DB8 00000000 NOP
B7514DBC 00000000 NOP
B7514DC0 00000000 NOP
B7514DC4 00000000 NOP
B7514DC8 00000000 NOP
B7514DCC 00000000 NOP
B7514DD0 00000000 NOP
B7514DD4 00000000 NOP
B7514DD8 00000000 NOP
B7514DDC 00000000 NOP
B7514DE0 00000000 NOP
B7514DE4 00000000 NOP
我参照的是北航的一本书TMS320C674 DSP应用开发,上面有类似例程。。。我是利用AISgen把应用程序生成.bin文件,然后打算将.bin文件烧写到flash里
不太明白您的意思,能否过程步骤具体点。。。是我要先把应用程序下载到DSP里,不用烧写应用工程吧???????????您说的交互窗口是AISgen吗?这个是手动 打开这个软件吧? ?我截图给您麻烦您给看一下,万分感谢啦!!!!!!!
交互窗口是用程序编的吗?我看书上的程序没有相关的啊,我把程序传附件里,麻烦帮我扫一眼,谢谢!!!!!!!!!!
/* * Core 6747 ' SDRAM. * All by yanxu. */ #define FILE2FLASH "11" #include "C6747.h" #include "C6747_flash.h" unsigned int k; void main( void ) { Uint32 i= 0; Uint32 error = 0; Uint32 length_to_burn = 0; Uint32 length_left = 0; FILE *fp; Uint32 dst=0; Uint8 tx[spiflash_PAGESIZE]; Uint8 rx[spiflash_PAGESIZE]; int file_start,file_end,file_length; int pos = 0; C6747_init(); spiflash_init(); spiflash_init(); printf("Start to write the SPI Flash...\n"); //step1:����д���ļ��Ƿ���� fp = fopen(FILE2FLASH,"rb"); if(fp == NULL) { // printf("\tThe file is not exist! \n"); exit(0); } printf("\tstep(1/3):flie checking:ok\n\n"); //step2:����ļ���С������Flash fseek(fp,0,0); fgetpos(fp, & file_start); fseek(fp,0,2); fgetpos(fp, & file_end); file_length = file_end-file_start; printf("\tstep(2/3):flie erase start...\n"); for(i=0;i<1+file_length/(64*1024);i++) spiflash_block_erase(i); printf("\t\tflash erase:ok\n\n"); //step3�����ļ�д��FLASH printf("\tstep(3/3):Flashing,wait....\n"); length_left= file_length; rewind(fp); fgetpos(fp, & pos); while(pos != file_end) { if(length_left > 256) length_to_burn = 256; else length_to_burn = length_left; fread(tx,1,length_to_burn,fp); fgetpos(fp, & pos); spiflash_write((Uint32)tx,(Uint32)dst,length_to_burn); spiflash_read((Uint32)dst,(Uint32)rx,length_to_burn); for(i=0;i<length_to_burn;i++) { if(tx[i]!=rx[i]) error++; } dst+=length_to_burn; length_left=length_left-length_to_burn; } fclose(fp); if(error) printf("\t\tburn failed\n"); else printf("congratulations!!!\n"); }
您好,我单步运行到
fp = fopen(FILE2FLASH,"rb");这句话时,再进行单步运行还是会跳到如下Disassembly窗口::,不知道到底什么原因
00712144 0001E000 IDLE
00712148 008A BNOP.S1 0x712144 (PC+4 = 0x00712144),0
0071214A 8C6E NOP 5
0071214C 3577 STW.D2T2 B10,*B15--[2]
0071214E 2C6E NOP 2
00712150 BC35 STW.D2T2 B3,*B15[1]
00712152 2C6E NOP 2
00712154 0503802A MVK.S2 0x0700,B10
00712158 0500786A MVKH.S2 0xf00000,B10
0071215C E3808000 .fphead n, l, W, BU, br, nosat, 0011100
00712160 0C6E NOP 1
00712162 9506 MV.L1X B10,A4
00712164 1008DA13 || CALLP.S2 0x716830 (PC+18128 = 0x00716830),B3
00712168 0627 || MVK.L2 0,B4
0071216A 1F12 || MVK.S1 152,A6
0071216C 10003592 CALLP.S2 0x71230C (PC+428 = 0x0071230c),B3
00712170 00282286 LDHU.D2T2 *+B10[1],B0
00712174 00006000 NOP 4