This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

移植 UBIFS ubuntu 到 am335x

Hello Ti

我使用 am335x 客製板

不得已非得用 ubuntu 系統, SD 卡開機成功!

燒成 UBFIS 形式,卻卡住無法登入,感覺是 ubuntu 某種行為是 for sd 卡,沒有 nand flash,log 訊息如下:

Detected MACID=d0:39:72:6b:d0:cd
[    6.340759] cpsw: Detected MACID = d0:39:72:6b:d0:cf
[    6.347320] omap_rtc am33xx-rtc: setting system clock to 2000-01-01 00:00:01 UTC (946684801)
[    6.762695] UBIFS: mounted UBI device 0, volume 0, name "rootfs"
[    6.769134] UBIFS: file system size:   204890112 bytes (200088 KiB, 195 MiB, 397 LEBs)
[    6.777557] UBIFS: journal size:       10452992 bytes (10208 KiB, 9 MiB, 21 LEBs)
[    6.785491] UBIFS: media format:       w4/r0 (latest is w4/r0)
[    6.791656] UBIFS: default compressor: lzo
[    6.796020] UBIFS: reserved for root:  0 bytes (0 KiB)
[    6.809753] VFS: Mounted root (ubifs filesystem) on device 0:13.
[    6.816650] Freeing init memory: 236K
[    8.480834] init: ureadahead main process (755) terminated with status 5

請問哪些論壇可以提供移植 UBIFS 的 ubuntu 資訊,或者可以直接提供 filesystem 給我,萬分感謝。