This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6636芯片3D加速器使用问题

TI工程师,您好:
在C6670芯片中,测试一个TCP3D加速器处理一个5696大小的码块,需要时间是60us左右。如果是在2*2天线MIMO的情况下,60us可接收空口数据是1.3个5696大小的码块,所以对于一个空口的MIMO,仅一个3D处理是赶不上空口速度的。在C6636芯片中,有两个TCP3D加速器,如果想用一片c6636处理2*2的MIMO,也就是一个节点的两个方向分别使用一个3D加速器来处理,基于前面分析,一个方向使用1个3D加速器是赶不上空口接收的速度,请问一片c6636芯片的解码加速器能否满足MIMO的需求?如果能满足应该怎样使用两个3D加速器?能否给一个详细的解答或3D在MIMO时使用的简单应用方案?期待你的答复,谢谢!

  • 每个TCP3D的throughput参考如下手册,8次迭代LTE mode大概在118Mbps。6636 TCP3D与6670的是一样,可以将多个TCP3d用起来,对于MIMO接收机而言,就是需要处理多个数据流,数据量大了,分别将多个cb块放到TCP3D处理即可。

    http://www.ti.com/general/docs/lit/getliterature.tsp?baseLiteratureNumber=sprabk5&fileType=pdf