This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6678: SPI boot模式在30度以下能正常工作,大于45度无法正常加载

Part Number: TMS320C6678


boot的时序如图:

最下面的是DSP返回的resetstate ,看上去DSP似乎完成了复位,但没有正确运行位于SPI FLASH中的程序。然而常温下捕获到同样的时序但dsp可以正常运行。

使用仿真器加入后程序可以正常运行,测试flash在55度下能正常工作。

另外启动GPIO设置为:16'b0001010000001101;

请问还有那些信号需要关注?