This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

blackhawk xds560v2仿真器驱动



Hi,

我拿到一块开发板TMDSEVM6678LE,但没有上面的blackhawk xds560v2仿真器驱动,请问哪里能下到这个驱动,或者谁能发给我一份?我的邮箱:flyingwonder@163.com

谢谢!

  • 这个驱动是包含在CCSV4以及以后版本中的。安装的时候,选择安装blackhawk 仿真器启动即可。

  • Hi, Titan

    我安装时选择了blackhawk仿真器驱动,但连上EVM板时,系统还是提示找不到驱动。

    我看别人安装好了能在设备管理器中看到该设备:

    但我的电脑里找不到

  • 打开CCS,检查target configuration中是否有这个blackhawk的仿真器驱动?另外,CCS的版本是多少?

  • 你可以重新下载新版本的CCS,然后注意安装时候,安装路径设置一个新的路径。然后选中blackhawk仿真器。应该没问题的。

  • 我的CCS版本是5.5,。根据CCS的安装结果,blackhawk的驱动应该是安装好了,但设备管理器中显示驱动没有正确安装。


  • CCS应该是安装好了,和板子链接的时候出现的什么错误?

    target configuration中有一个TEST按钮,可以测试通过吗?

  • 设备管理器中有叹号,我始终觉得仿真器驱动没有安装好啊。板子的运行时的图片如下:

    在CCS中,Test Connection的结果如下:

    [Start]

    Execute the command:

    %ccs_base%/common/uscif/dbgjtag.exe -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity

    [Result]


    -----[Print the board config pathname(s)]------------------------------------

    C:\Users\comeback\AppData\Local\.TI\4084209646\
    0\0\BrdDat\testBoard.dat

    -----[Print the reset-command software log-file]-----------------------------

    This utility has selected a 560/2xx-class product.
    This utility will load the program 'bh560v2u.out'.
    E_RPCENV_IO_ERROR(-6) No connection: emulator was not found
    Download failed for file D:\ti\ccsv5\ccs_base\common\uscif\xds560v2.out

    An error occurred while soft opening the controller.

    -----[An error has occurred and this utility has aborted]--------------------

    This error is generated by TI's USCIF driver or utilities.

    The value is '-250' (0xffffff06).
    The title is 'SC_ERR_ECOM_EMUNAME'.

    The explanation is:
    An attempt to access the named emulator via USCIF ECOM has failed.

    [End]

  • 谁能把EVM板附带的光盘里的仿真器驱动发我一份啊?

  • 到问题了,应该是我系统有问题。我把TI相关的软件包括CCS5.5,还有seed的仿真器驱动全部卸载了,然后再重装了CCS 5.5,系统就能正常识别仿真器了。

  • 恩,恭喜问题解决。昨下午有事出去办事。一般出现这个错误:The explanation is:
    An attempt to access the named emulator via USCIF ECOM has failed.

    就非常可能是系统的问题,在win7上一般都能够稳定解决的。

  • 你好,我是在linux上安装的CCS v5.5 ,linux版本是ubuntu 14.04,连接的板子是TMDSEVM6678LE,也出现了同样的问题。同时,consol显示i:IcePick_D: Error initializing emulator: (Error -2083 @ 0x0) Unable to communicate with the emulator. Confirm emulator configuration and connections, reset the emulator, and retry the operation. (Emulation package 5.1.232.0) ,test connection的显示与主贴一致,也是因为系统的问题吗?

    在target configuration中可以找到blackhawk XDS560 v2,我准备重安下驱动,不知道可行吗?可以在哪里下到这个驱动呢?

    谢谢