Hi,
我拿到一块开发板TMDSEVM6678LE,但没有上面的blackhawk xds560v2仿真器驱动,请问哪里能下到这个驱动,或者谁能发给我一份?我的邮箱:flyingwonder@163.com
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
设备管理器中有叹号,我始终觉得仿真器驱动没有安装好啊。板子的运行时的图片如下:
在CCS中,Test Connection的结果如下:
[Start]
Execute the command:
%ccs_base%/common/uscif/dbgjtag.exe -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
C:\Users\comeback\AppData\Local\.TI\4084209646\
0\0\BrdDat\testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 560/2xx-class product.
This utility will load the program 'bh560v2u.out'.
E_RPCENV_IO_ERROR(-6) No connection: emulator was not found
Download failed for file D:\ti\ccsv5\ccs_base\common\uscif\xds560v2.out
An error occurred while soft opening the controller.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-250' (0xffffff06).
The title is 'SC_ERR_ECOM_EMUNAME'.
The explanation is:
An attempt to access the named emulator via USCIF ECOM has failed.
[End]
你好,我是在linux上安装的CCS v5.5 ,linux版本是ubuntu 14.04,连接的板子是TMDSEVM6678LE,也出现了同样的问题。同时,consol显示i:IcePick_D: Error initializing emulator: (Error -2083 @ 0x0) Unable to communicate with the emulator. Confirm emulator configuration and connections, reset the emulator, and retry the operation. (Emulation package 5.1.232.0) ,test connection的显示与主贴一致,也是因为系统的问题吗?
在target configuration中可以找到blackhawk XDS560 v2,我准备重安下驱动,不知道可行吗?可以在哪里下到这个驱动呢?
谢谢