This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: Pcie rescan crash, Two tda4vm soc, one is rc, one is ep

Part Number: TDA4VM


Hi Sir:

My costromer board is two TDA4VM SOC, and  soc1 is pcie3 rc  , soc2 is pcie3 ep. 

linux SDK is 8.04.

And the Hardware SCH is this

When soc1 and soc2 power on,  soc1 lspci can see 0x104c:b00d soc2 bridge device,   and soc1 echo 1 > /sys/bus/pci/devices/0000:00:00.0/remove , echo 1 > /sys/bus/pci/rescan ok.

But the problem is :  After i creat Endpot function in soc2 (ep devcie) , and then in soc1(rc)  echo 1 > /sys/bus/pci/devices/0000:00:00.0/remove , echo 1 > /sys/bus/pci/rescan, the soc1 system crash immediately.

log is this:

..... My Operating Steps: 

soc2: 

cd /sys/kernel/config/pci_ep
mkdir functions/pci_epf_test/func1
echo 0x104c > functions/pci_epf_test/func1/vendorid
echo 0xb00d > functions/pci_epf_test/func1/deviceid
echo 12 > functions/pci_epf_test/func1/msi_interrupts
echo 12 > functions/pci_epf_test/func1/msix_interrupts
ln -s functions/pci_epf_test/func1 controllers/2930000.pcie-ep
echo 1 > controllers/2930000.pcie-ep/start

soc1:

echo 1 > /sys/bus/pci/devices/0000:00:00.0/remove
echo 1 > /sys/bus/pci/rescan

 

Dts setting:

soc1:

&pcie3_rc {
/*reset-gpios = <&exp2 20 GPIO_ACTIVE_HIGH>;*/
phys = <&serdes3_pcie_link>;
phy-names = "pcie-phy";
num-lanes = <2>;
};

&serdes3 {
assigned-clocks = <&serdes3 CDNS_SIERRA_PLL_CMNLC>;
assigned-clock-parents = <&wiz3_pll1_refclk>;

serdes3_pcie_link: phy@0 {
reg = <0>;
cdns,num-lanes = <2>;
#phy-cells = <0>;
cdns,phy-type = <PHY_TYPE_PCIE>;
resets = <&serdes_wiz3 1>, <&serdes_wiz3 2>;
};
};

soc2:

&pcie3_ep {
/delete-property/ power-domains;
phys = <&serdes3_pcie_link>;
phy-names = "pcie-phy";
num-lanes = <2>;
};

&serdes3 {
assigned-clocks = <&serdes3 CDNS_SIERRA_PLL_CMNLC>;
assigned-clock-parents = <&wiz3_pll1_refclk>;

serdes3_pcie_link: phy@0 {
reg = <0>;
cdns,num-lanes = <2>;
#phy-cells = <0>;
cdns,phy-type = <PHY_TYPE_PCIE>;
resets = <&serdes_wiz3 1>, <&serdes_wiz3 2>;
};
};

...............................

So, what reason can is?   like refclk setting ? etc...

How can I do ......