Part Number: TDA4VM
您好
我们尝试在TDA4VM上添加MAXIM摄像头和解串器,遇到一些问题,情况如下:
1、SDK版本
ti-processor-sdk-linux-j7-evm-08_06_00_11
ti-processor-sdk-rtos-j721e-evm-08_06_00_12
2、视频链路,使用MAX96712的EVK板通过CSI接口接入到TDA4VM评估板上
AR0147+MAX96705+MAX96712-->CSI -->TDA4VM
3、我们可以通过IIC读写MAX96712和MAX96705的寄存器
4、参考TI文档Adding new image sensor to PSDK RTOS章节,尝试增加了AR0147的摄像头,按照流程编译安装成功,在运行vision_app_init.sh正常,考虑使用run_app_single_cam.sh验证摄像头是否添加正确?
问题1、如果考虑使用run_app_single_cam.sh,CSIRX部分是否需要改动
2、看到TI当前sensor_drv都是基于UB960和UB970解串器添加摄像头,是否有基于MAXIM的demo可以参考
3、如果不适用TI的sensor框架,直接使用IIC设置解串器和摄像头,然后使用CSIRX去获取vedio是否可行,以及需要注意什么内容