hello,
I wanna boot my board from the second net card, but the uboot can't find it,
there is the Uboot boot log:
.....
TI8168-GP rev 2.1
ARM clk: 987MHz
DDR clk: 796MHz
I2C: ready
DRAM: 2 GiB
NAND: HW ECC BCH8 Selected
256 MiB
MMC: OMAP SD/MMC: 0
Net: Detected MACID:50:56:63:a7:8d:a5
Ethernet PHY: GENERIC @ 0x01
DaVinci EMAC
Hit any key to stop autoboot: 0
....
when i powered on. it seems like not configure the eth1 in Uboot .
what should I do, or any reference for this problem. thanks ..