This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hello,
I wanna boot my board from the second net card, but the uboot can't find it,
there is the Uboot boot log:
.....
TI8168-GP rev 2.1
ARM clk: 987MHz
DDR clk: 796MHz
I2C: ready
DRAM: 2 GiB
NAND: HW ECC BCH8 Selected
256 MiB
MMC: OMAP SD/MMC: 0
Net: Detected MACID:50:56:63:a7:8d:a5
Ethernet PHY: GENERIC @ 0x01
DaVinci EMAC
Hit any key to stop autoboot: 0
....
when i powered on. it seems like not configure the eth1 in Uboot .
what should I do, or any reference for this problem. thanks ..
现在,已经可以从eth0 NFS启动了,启动之后也可以通过
$ ifconfig eth1 192.168.1.xxx
$ifup eth1 来启用
因为硬件工程师那边希望能用eth1来作为首选网口。我想这应该是需要修改Uboot的配置项,但是现在不知道到那里修改,根据Uboot启动的输出,可以查到相关的实现函数,但是不知道怎么配置。搜索到一个帖子,但是没有说的太明白:
http://e2e.ti.com/support/embedded/linux/f/354/t/332458.aspx
http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/717/t/231814.aspx
thank again.