This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

nfs: server 192.168.0.90 not responding, still trying



DM365 EVM :>boot

TFTP from server 192.168.0.86; our IP address is 192.168.0.88

Filename 'uImage_ipnc_DM365_EVM'.

Load address: 0x80700000

Loading: *#################################################################

#################################################################

#################################################################

#################################################################

#################################################################

########################################

done

Bytes transferred = 1866840 (1c7c58 hex)

## Booting kernel from Legacy Image at 80700000 ...

   Image Name:   Linux-2.6.18_pro500-davinci_IPNC

   Image Type:   ARM Linux Kernel Image (uncompressed)

   Data Size:    1866776 Bytes =  1.8 MB

   Load Address: 80008000

   Entry Point:  80008000

   Verifying Checksum ... OK

   Loading Kernel Image ... OK

OK

 

Starting kernel ...

 

Uncompressing Linux............................................................................................................................ done, booting the kernel.

Linux version 2.6.18_pro500-davinci_IPNC_DM36x_2.6.0 (root@localhost.localdomain) (gcc version 4.2.0 (MontaVista 4.2.0-16.0.32.0801914 2008-08-30)) #1 PREEMPT Tue Apr 10 17:47:14 CST 2012

CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177

Machine: DaVinci DM365 EVM

Memory policy: ECC disabled, Data cache writeback

DaVinci DM0365 variant 0x8

PLL0: fixedrate: 24000000, commonrate: 121500000, vpssrate: 243000000

PLL0: vencrate_sd: 27000000, ddrrate: 243000000 mmcsdrate: 121500000

PLL1: armrate: 297000000, voicerate: 99000000, vencrate_hd: 74250000

CPU0: D VIVT write-back cache

CPU0: I cache: 16384 bytes, associativity 4, 32 byte lines, 128 sets

CPU0: D cache: 8192 bytes, associativity 4, 32 byte lines, 64 sets

Built 1 zonelists.  Total pages: 12288

Kernel command line: console=ttyS0,115200n8 noinitrd rw ip=192.168.0.88 root=/dev/nfs nfsroot=192.168.0.90:/home/hexiaojun/ipnc26-orig/ipnc/target/filesys,nolock mem=48M eth=64:43:46:00:00:09

TI DaVinci EMAC: kernel boot params Ethernet address: 64:43:46:00:00:09

PID hash table entries: 256 (order: 8, 1024 bytes)

Clock event device timer0_0 configured with caps set: 07

Console: colour dummy device 80x30

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory: 48MB = 48MB total

Memory: 44568KB available (3193K code, 656K data, 184K init)

Security Framework v1.0.0 initialized

Capability LSM initialized

Mount-cache hash table entries: 512

CPU: Testing write buffer coherency: ok

NET: Registered protocol family 16

MUX: initialized SPI0_SCLK

MUX: initialized SPI0_SDO)

MUX: initialized SPI0_SDI

MUX: initialized SPI0_SDENA0

DaVinci: 104 gpio irqs

MUX: initialized GPIO20

MUX: initialized I2C_SCL

Generic PHY: Registered new driver

ch0 default output "COMPOSITE", mode "NTSC"

VPBE Encoder Initialized

SCSI subsystem initialized

NET: Registered protocol family 2

IP route cache hash table entries: 512 (order: -1, 2048 bytes)

TCP established hash table entries: 2048 (order: 1, 8192 bytes)

TCP bind hash table entries: 1024 (order: 0, 4096 bytes)

TCP: Hash tables configured (established 2048 bind 1024)

TCP reno registered

VFS: Disk quotas dquot_6.5.1

Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)

squashfs: version 3.1 (2006/08/19) Phillip Lougher

JFFS2 version 2.2. (NAND) (C) 2001-2006 Red Hat, Inc.

yaffs Apr 10 2012 17:44:58 Installing. 

SGI XFS with no debug enabled

Initializing Cryptographic API

io scheduler noop registered

io scheduler anticipatory registered (default)

LTT : ltt-facilities init

LTT : ltt-facility-core init in kernel

DAVINCI-WDT: DaVinci Watchdog Timer: heartbeat 60 sec

Serial: 8250/16550 driver $Revision: 1.90 $ 2 ports, IRQ sharing disabled

serial8250.0: ttyS0 at MMIO map 0x1c20000 mem 0xfbc20000 (irq = 40) is a 16550A

serial8250.0: ttyS1 at MMIO map 0x1d06000 mem 0xfbd06000 (irq = 41) is a 16550A

RAMDISK driver initialized: 1 RAM disks of 32768K size 1024 blocksize

Davinci EMAC MII Bus: probed

MAC address is 00:0e:99:03:50:f2

TI DaVinci EMAC Linux version updated 4.0

netconsole: not configured, aborting

Linux video capture interface: v2.00

Trying to register davinci display video device.

layer=c0588e00,layer->video_dev=c0588f60

Trying to register davinci display video device.

layer=c0588c00,layer->video_dev=c0588d60

davinci_init:DaVinci V4L2 Display Driver V1.0 loaded

i2c /dev entries driver

nand_davinci nand_davinci.0: Using 4-bit hardware ECC

NAND device: Manufacturer ID: 0x2c, Chip ID: 0xd3 (Micron NAND 1GiB 3,3V 8-bit)

2 NAND chips detected

Bad block table not found for chip 0

Bad block table not found for chip 1

Bad block table not found for chip 0

Bad block table not found for chip 1

Scanning device for bad blocks

Scanning device for bad blocks

Creating 6 MTD partitions on "nand_davinci.0":

0x00000000-0x003c0000 : "bootloader"

0x003c0000-0x00400000 : "params"

0x00400000-0x00800000 : "kernel"

0x00800000-0x20800000 : "filesystem1"

0x20800000-0x20c00000 : "filesystem2"

0x20c00000-0x80000000 : "filesystem3"

nand_davinci nand_davinci.0: hardware revision: 2.3

musb_hdrc: version 6.0, cppi-dma, peripheral, debug=0

MUX: initialized GPIO33

musb_hdrc musb_hdrc: No DMA interrupt line

musb_hdrc: USB Peripheral mode controller at c381c000 using DMA, IRQ 12

rtc_davinci_dm365 rtc_davinci_dm365.0: rtc intf: proc

rtc_davinci_dm365 rtc_davinci_dm365.0: rtc intf: dev (254:0)

rtc_davinci_dm365 rtc_davinci_dm365.0: rtc core: registered rtc_davinci_dm365 as rtc0

davinci-mmc davinci-mmc.0: Supporting 4-bit mode

davinci-mmc davinci-mmc.0: Using DMA mode

Advanced Linux Sound Architecture Driver Version 1.0.12rc1 (Thu Jun 22 13:55:50 2006 UTC).

ASoC version 0.13.1

CQ0093 Voice Codec 0.1

asoc: cq93vc <-> davinci-vcif mapping ok

ALSA device list:

  #0: On-chip voice codec (cq93vc)

IPv4 over IPv4 tunneling driver

TCP bic registered

NET: Registered protocol family 1

NET: Registered protocol family 17

Time: timer0_1 clocksource has been installed.

Clock event device timer0_0 configured with caps set: 08

Switched to high resolution mode on CPU 0

rtc_davinci_dm365 rtc_davinci_dm365.0: setting the system clock to 2000-01-01 00:00:00 (946684800)

IP-Config: Guessing netmask 255.255.255.0

IP-Config: Complete:

      device=eth0, addr=192.168.0.88, mask=255.255.255.0, gw=255.255.255.255,

     host=192.168.0.88, domain=, nis-domain=(none),

     bootserver=255.255.255.255, rootserver=192.168.0.90, rootpath=

Looking up port of RPC 100003/2 on 192.168.0.90

Looking up port of RPC 100005/1 on 192.168.0.90

VFS: Mounted root (nfs filesystem).

Freeing init memory: 184K

 

INIT: version 2.86 booting

 

0

Starting the hotplug events dispatcher: udevd.

Synthesizing the initial hotplug events...done.

Waiting for /dev to be fully populated...done.

0

CSL: Module install successful, device major num = 253 

CSL: Module version 0.10.00, built on Apr 10 2012 17:49:26 

I2C: Module install successful, device major num = 252 

DMA: Module install successful, device major num = 251 

MUX: initialized GPIO40

DRV: Sensor interface selected on DM365 EVM

DRV: Module install successful

DRV: Module built on Apr 10 2012 17:49:30 

DRV: EDMACC.QUEPRI  = 00000777

DRV: SYSTEM.MSTPRI0 = 00440022

DRV: SYSTEM.MSTPRI1 = 00000244

DRV: ISP.BCR        = 00000002

DRV: SYSTEM.MISC    = 00000399

CMEMK module: built on Apr 10 2012 at 17:48:45

  Reference Linux version 2.6.18

  File /home/hexiaojun/ipnc26-orig/dvsdk_2_10_01_18/linuxutils_2_24_03/packages/ti/sdo/linuxutils/cmem/src/module/cmemk.c

allocated heap buffer 0xc4000000 of size 0x5000000

CMEM Range Overlaps Kernel Physical - allowing overlap

CMEM phys_start (0x1000) overlaps kernel (0x80000000 -> 0x83000000)

cmemk initialized

EDMAK module: built on Apr 10 2012 at 17:48:48

  Reference Linux version 2.6.18

  File /home/hexiaojun/ipnc26-orig/dvsdk_2_10_01_18/linuxutils_2_24_03/packages/ti/sdo/linuxutils/edma/src/module/edmak.c

IRQK module: built on Apr 10 2012 at 17:48:49

  Reference Linux version 2.6.18

  File /home/hexiaojun/ipnc26-orig/dvsdk_2_10_01_18/linuxutils_2_24_03/packages/ti/sdo/linuxutils/irq/src/module/irqk.c

irqk initialized

Creat queue id:0

queue id:0

FileMngThread created

Creat queue id:32769

queue id:32769

AlramThread created

Share memory init success

queue id:32769

Creat queue id:65538

queue id:65538

Creat queue id:98307

queue id:98307

IPNC_DM36x_2.6.0 (root@localhost.localdomain) (gcc version 4.2. 

queue id:65538

Check_device_version : read device error !!

 

CPU is DM365

./av_server.out DM365 NTSC APPRO2A AEWB 720P H264 5000000 VBR AUTO MENUOFF &

Starting mounting local filesystems: mount 

AVSERVER UI: Initializing.

none on /dev/shm type tmpfs (rw,size=5M)

none on /var/run type tmpfs (rw)

none on /tmp type tmpfs (rw,sync)

 

 CLK Hz,

 ARM   Hz =  297000000

 DDR   Hz =  243000000

 VPSS  Hz =  243000000

 IMCOP Hz =  243000000

 

 [OSA_FILE ] Reading file [/mnt/nand/IMG_Paramset.bin] ... ERROR 

 

IMAGE TUNE: Paramset File is not available..... Setting DEFAULT parameter

Setting up networking ...ApproDrvInit: 7

Creat queue id:131076

queue id:131076

 

CONFIGURING AVSERVER FOR DM365 .....

queue id:65538

SENSOR FPS VALUE = 30

queue id:131076

DavinciDisplay DavinciDisplay.1: Before finishing with S_FMT:

layer.pix_fmt.bytesperline = 640,

 layer.pix_fmt.width = 640, 

 layer.pix_fmt.height = 480, 

 layer.pix_fmt.sizeimage =460800

 

 

 FR : 0 usersDavinciDisplay DavinciDisplay.1: pixfmt->width = 640,

 layer->layer_info.config.line_length= 640

 registered from exsiting face album

IPNC_DM36x_2.6.0 (root@localhost.localdomain) (gcc version 4.2. 

IPNC AUTO_IRIS = 1 

.

Starting hotplug subsystem:

   pci     

   pci      [success]

   usb     

   usb      [success]

   isapnp  

   isapnp   [success]

   ide     

Simple mixer control 'PGA',0

  Capabilities: cvolume

  Capture channels: Mono

  Limits: Capture 0 - 3

  Mono: Capture 2 [67%]

Simple mixer control 'Mono DAC',0

  Capabilities: pvolume pvolume-joined

  Playback channels: Mono

  Limits: Playback 0 - 63

  Mono: Playback 47 [75%]

SystemInit success

Schedule manager init success

   ide      [success]

   input   

   input    [success]

   scsi    

   scsi     [success]

done.

Starting portmap daemon: portmap. 

Starting internet superserver: inetd.

io scheduler deadline registered

io scheduler cfq registered

 sbulla: unknown partition table

Installing knfsd (copyright (C) 1996 okir@monad.swb.de).

loop: loaded (max 8 devices)

tun: Universal TUN/TAP device driver, 1.6

tun: (C) 1999-2004 Max Krasnyansky <maxk@qualcomm.com>

CSLIP: code copyright 1989 Regents of the University of California

PPP generic driver version 2.4.2

PPP Deflate Compression module registered

g_file_storage gadget: no file given for LUN0

insmod: Loading iSCSI transport class v1.1-646.cannot insert `/opt/ipnc/modules/g_file_storage.ko': Invalid parameters (-1): Invalid argument

<5>iscsi: registered transport (tcp)

 sbulla: unknown partition table

mkdosfs 3.0.6 (04 Oct 2009)

unable to get drive geometry, using default 255/63

/dev/sbulla has 255 heads and 63 sectors per track,

logical sector size is 512,

using 0xf8 media descriptor, with 1024 sectors;

file system has 2 12-bit FATs and 4 sectors per cluster.

FAT size is 1 sector, and provides 247 clusters.

Root directory contains 512 slots.

Volume ID is 39a05e99, no volume label.

---start boot_proc--

queue id:0

umount: /mnt/mmc: not mounted

mount: special device /dev/mmcblk0 does not exist

mount: special device /dev/mmcblk0p1 does not exist

nfs: RPC call returned error 101

killall: dhcpcd:nfs: RPC call returned error 101

 no process killed

rm: cannot remove `/var/run/dhcpcd-eth0.pid': No such file or directory

net_search_gateway:eth0, 1A8C0, 0, 1

nfs: server 192.168.0.90 not responding, still trying

nfs: server 192.168.0.90 not responding, still trying

 

NFS能正常启动系统,但是最后却出现NFS没有响应,请教下是什么原因,谢谢!