This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

K2 Gigabit Ethernet (GbE) Switch Subsystem



k2 的Gigabit Ethernet (GbE) Switch Subsystem文档  关于 Serializer/Deserializer (SerDes) SGMII Boot Configuration Registers的偏移地址和基地址

让看数据手册,无法找到相关的详细文档。导致D:\TI\pdk_keystone2_3_00_03_15\packages\ti\platform\evmk2h\platform_lib\src\evmc66x_phy.c的CSL_SgmiiDefSerdesSetup函数全是寄存和偏移量的操作,不知道对应哪一个寄存器。

问题1:关于 Serializer/Deserializer (SerDes) SGMII Boot Configuration Registers的偏移地址和基地址是多少?

问题2:CSL_SgmiiDefSerdesSetup下对应的寄存器文档

问题3:我需要修改sgmii的PLL输入值,其控制寄存器的偏移地址和基地址是多少?

  • Table 3-169是KeyStone I的寄存器,你用的K2H 是KeyStone II. KeyStone II Serdes有专门的user guide.

    K2上的SGMII SerDes只支持156.25MHz和125MHz的输入时钟,相应的PLL配置也是固定的。直接调用CSL函数就可以了,不需要去研究具体的PLL寄存器.

    下面是一段代码供您参考:

    typedef struct
    {
    	CSL_SERDES_REF_CLOCK inputRefClock;
    
    	float linkSpeed_GHz; 	/*the max link speed of all lanes at GHz*/
    
    	/*bit 0~3 control the endable/disable of 4 lanes. 0: disable; 1: enable*/
    	Uint32 laneEnableMask; 
    
    	Uint32 internalLoopbackDisableMask;
    } K2_GE_SerdesConfig;
    
    char * SerdesErrorStr[]=
    {
    	"SERDES no error",
    	"SERDES error: invalid input reference clock speed!",
    	"SERDES error: invalid link speed!"
    };
    /*Serdes initialization for Giga bit ethernet*/
    void K2_GE_Serdes_init(K2_GE_SerdesConfig * serdes_cfg, Uint32 uiBase_addr)
    {
    	int i;
    	CSL_SERDES_LINK_RATE linkSpeed;
    	CSL_SERDES_LANE_CTRL_RATE laneRateScale;
    	Uint32 uiResult;
    
    	// Disable pll before configuring the SerDes registers
    	CSL_EthernetSerdesShutdown(uiBase_addr);
    
    	if(serdes_cfg->linkSpeed_GHz== 1.25f)
    	{
    		linkSpeed= CSL_SERDES_LINK_RATE_1p25G;
    		laneRateScale = CSL_SERDES_LANE_QUARTER_RATE; //???
    	}
    	else
    		printf("Error: link speed %.3fGbps is not supported by SGMII\n",serdes_cfg->linkSpeed_GHz);
    	
    	uiResult= CSL_EthernetSerdesInit(uiBase_addr,
    		serdes_cfg->inputRefClock, linkSpeed);
    	if(uiResult)
    		printf("  %s\n", SerdesErrorStr[uiResult]);
    
    	for(i=0; i<4; i++)
    	{
    		if((serdes_cfg->laneEnableMask>>i)&1)
    		{
    			CSL_EthernetSerdesLaneConfig(uiBase_addr,
    				serdes_cfg->inputRefClock, linkSpeed, i);
    		}
    	}
    
    	CSL_EthernetSerdesComEnable(uiBase_addr);
    
    	for(i=0; i<4; i++)
    	{
    		if((serdes_cfg->laneEnableMask>>i)&1)
    		{
    			uiResult= CSL_EthernetSerdesLaneEnable(uiBase_addr,
    				i, (serdes_cfg->internalLoopbackDisableMask>>i)&1, laneRateScale);
    			if(uiResult)
    				printf("  lane %d error: invalid rate scale\n", i);
    		}
    	}
    
    	// Enable pll via the pll_ctrl 0x0014
    	CSL_EthernetSerdesPllEnable(uiBase_addr);
    
    	// Wait the SerDes PLL lock
    	while(CSL_SERDES_STATUS_PLL_NOT_LOCKED==K2_SerdesPLLGetStatus(uiBase_addr));
    #if 0	
    	for(i=0; i<4; i++)
    	{
    		if(((serdes_cfg->laneEnableMask>>i)&1)&&((serdes_cfg->internalLoopbackDisableMask>>i)&1))
    		{
    			while(CSL_SERDES_STATUS_PLL_NOT_LOCKED==K2_SerdesLaneGetStatus(uiBase_addr, i));
    		}
    	}
    #endif
    }
    
    	 	K2_GE_Serdes_init(&serdes_cfg, CSL_NETCP_SERDES_CFG_REGS);
    

  • 您好,我使用的是K2e的评估板,运行的是masdk中的hello world例程,我运行后出现

    Registration of the EMAC successful,waiting for link up ..

    Service status:DHCPC  :Enables :  :000

    Service status DHCPC  :Enables:   :000

    此后,console中就再也没有任何提示,程序一直在运行,不会自动停止。相关的寄存器中是error,无法读取。

    请问,我需要修改哪些参数,才能正确运行程序,传输数据?

    此外,如何修改DSP的IP配置模式(DHCP 或是手动)?

    谢谢,期待您的回答

    hitzhaoliangyu@126.com