This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSP C6743 UART BOOT为什么在上电后用串口助手可以收到BOOTME,但在UART BOOT HOST里若勾选Wait for BOOTME却出现错误:(AIS Parse): Waiting for BOOTME... (power on or reset target now)

(File IO): Read 5940 bytes from file G:\DSP\MEMS3\flash_SPI\sdram\Debug\11.bin.
(Serial Port): Opening COM1 at 115200 baud...
(AIS Parse): Read magic word 0x41504954.
(AIS Parse): Waiting for BOOTME... (power on or reset target now)
(Serial Port): Read error! (The operation has timed out.)
(AIS Parse): Read invalid BOOTME string.
(AIS Parse): Boot aborted.
(Serial Port): Closing COM1.

  • 你好,请问是谁的板子,在用串口工具查看的时候,看是不是BOOTME前面有个其它信号或0之类的。

    另外,也可以不断电情况下,手动复位芯片看是否也会有同样问题。