This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请问为什么C6743 UART BOOT在AISgen没有使能CRC、UART BOOT HOST 里没有勾选Wait for BOOTME情况下,有时好使,有时不好使,不好使时出现如下错误:

补充:在使能CRC、UART BOOT HOST 里勾选Wait for BOOTME情况下一直不好使

(File IO): Read 5900 bytes from file G:\DSP\MEMS3\flash_SPI\sdram\Debug\11.bin.

(Serial Port): Opening COM1 at 115200 baud...
(AIS Parse): Read magic word 0x41504954.
(AIS Parse): Performing Start-Word Sync...
(Serial Port): Read error! (The operation has timed out.)
(AIS Parse): I/O Error in read!
(AIS Parse): Boot aborted.
(Serial Port): Closing COM1.

  • 不勾选的情况下,就是不等bootme信号,直接发数据,如果这时CPU没有timer out可能会成功,过了timer out时间就不会再接收上位机发的数据了,所以这样是不确定的。