This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dm8168 ezsdk nand 烧写

你好:

    我想问一下,8168的NAND烧写。如何用CCSV5进行烧写。根据WIKI上的烧写方式,有两个问题:

1:   当使用BCH 8BIT烧写时,烧写不进去。一直出现

Attempting to start write in block number 0x2B1.
Writing image data to Block 689 Page0x0
Verify failed. Attempting to clear page
Attempting to start write in block number 0x2B2.

2: 当使用HAM烧写时,是可以烧写完成,也打印出烧写成功。但是上电从NAND启动时,终端上什么显示也没有。

 

我看SD启动时,里面有MLO,BOOT.SRC文件,这些文件是否也需要一起烧写进去。如果是的话应该如何烧写。

谢谢!